MPLAB® Harmony v3 Peripheral Libraries on SAM L10: Step 1
Install the MPLAB® Code Configurator (MCC) Plug-in in MPLAB X IDE
Verify that MCC is installed.
• Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open.
• Go to Tools > Embedded > MPLAB® Code Configurator v5: Open/Close.

Create MPLAB Harmony v3 Project using MPLAB X IDE
In the Categories pane of the New Project dialog window, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

In the Framework Path edit box, browse to the folder you downloaded the framework to. Then click Next.

In the Project Settings window, apply the following settings:
Location: indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example, C:\microchip\harmony\v3\training\dev.
- Folder: indicates the name of the MPLAB X IDE .X folder. Enter "sam_l10_xpro" to create a sam_l10_xpro.X folder.
- Name: enter the project’s logical name as "getting_started_sam_l10_xpro". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to configuration settings.


Follow the steps below to set the project’s Configuration Settings:
Name: enter the configuration name as "sam_l10_xpro".
- Target Device: select ATSAML10E16A as the target device.
- After selecting the target device, click Finish to launch the MCC.

After launching, the MCC content manager window will display. Click Select MPLAB Harmony (by default this option is selected).

Click Finish to launch the MCC tool with the packages.

The MCC plugin’s main window for the project will be displayed.

Before proceeding, set up the compiler toolchain. Click on the File tab on the top left pane, then click Project Properties (getting_started_sam_l10_xpro).

Make sure that XC32 (v4.30) is selected as the Compiler Toolchain for XC32. Additionally, select Simulator from the drop-down.
Click on Apply and then click on OK.

Verify Clock Settings
Launch Clock Easy View by going to the Project Graph tab in MPLAB X IDE and then selecting Plugins > Clock Configuration.

A new window, Clock Easy View, is opened in the project’s main window.
Click on the Clock Easy View tab, scroll to the right and verify that the Main Clock is set to 32 MHz.