Update and Configure an Existing MHC-based MPLAB® Harmony v3 Project to MCC-based Project: Step 1
Contents
Step 1.1: Open MPLAB® Harmony v3 Project in MPLAB X IDE
Download the pre-developed project to your computer. The ZIP file contains the MHC project which will be updated and configured using the MPLAB® Code Configurator (MCC).
Launch MPLAB X IDE from the Windows® Start Menu. Close any projects and files that are currently open. Go to Files > Open Project.
You will get an Open Project pop-up window. Select the project pic32mz_ef_curiosity_v2.X from the project download path.
Click image to enlarge.
Right-click on the getting_started_ext_pic32mz_ef_curiosity_v2 project and select Set as Main Project.
Step 1.2: Migrate to MCC project
Before proceeding further, make sure the Harmony Content Path is set properly. Harmony Content Path is where you have downloaded the Harmony repositories.
On MPLAB X IDE, go to Tools > Options. After opening the Options window, go to Plugins and set the proper Harmony Content Path.
Open MCC.

Click on the MCC icon in the IDE main toolbar, or go to Tools > MPLAB Code Configurator v4: Open/Close.
![]()
Import the MHC project to MCC by clicking the Yes button on the pop-up window.

MCC starts loading the existing MHC configuration database. Wait for this step to complete.

After successful loading, MCC opens the Project Graph, Resource Management, and Configuration Options windows.
Step 1.3: Verify the Clock Settings
Launch the Clock Diagram by going to Clock Configuration under the Plugins: drop-down option in the Project Graph of MCC. A new window, Clock Diagram, is opened in the project’s main window.
Click on the Clock Diagram tab, scroll to the right and verify that the SYSCLK is set to 200 MHz.
Tool Tip: Double-click on the Clock Diagram tab to maximize the window.