Update and Configure an Existing MHC-based MPLAB® Harmony v3 Project to MCC-based Project: Step 3
In this step, we will extend the MPLAB® Harmony Configurator (MHC) project by configuring a GPIO pin for the SW3 switch and user LED (LED3).
Step 3.1: Configure the Switch Button Pin
Configure the switch button, BTN3 pin, with a General Purpose Input/Output (GPIO) interrupt handler.
The switch button, BTN3, will be configured as per the design schematic of the Curiosity PIC32MZ EF 2.0 Development Board.

Open Pin Configuration under Plugins: to verify the pin configuration. Select the Pin Settings tab and sort (Order) the entries by Ports.

Scroll down to GPIO pin RJ6 (Pin #133) in the Pin ID column and configure RJ6 as a GPIO pin for SW3 switch functionality. An internal pull-up is enabled to avoid false edge detection as there is no external pull-up on the Curiosity PIC32MZ EF 2.0 Development Board.

Step 3.2: Configure the LED Pin
The user LED3 will be configured as per the design schematic of the Curiosity PIC32MZ EF 2.0 Development Board.

Select the Pin Settings tab and then scroll down to GPIO pin RJ3 (Pin #117) in the Pin ID column and configure RJ3 as an output pin for LED3 functionality.