Getting Started with USB on SAM MCUs Using MPLAB® Harmony v3: Step 1
Create and Configure Harmony v3 Project
Install the MPLAB® Code Configurator (MCC) Plug-in in MPLAB X IDE
Verify that MPLAB Code Configurator (MCC) is installed.
- Launch MPLAB X IDE.
- Go to Tools > Embedded.
- You will see MPLAB Code Configurator v5 in the menu.

Figure 1: Check if Harmony 3 Plug-in is installed
Create MPLAB Harmony v3 Project Using MPLAB X IDE
Select File > New Project from the IDE main menu or click on the New Project button
.
In the Categories pane of the New Project dialog, select Microchip Embedded. In the Projects pane, select 32-bit MCC Harmony Project, then click Next.

Figure 2: Select 32-bit MCC Harmony Project
In the Framework Path edit box, browse to the folder you downloaded the framework to, then click Next.

Figure 3: Verify Framework Path
In the Project Settings window, apply the following settings:
Location: Indicates the path to the root folder of the new project. All project files will be placed inside this folder. The project location can be any valid path, for example: C:\Projects\getting_started_drivers_middleware.
- Folder: Indicates the name of the MPLAB X Project .X folder. Enter "sam_e70_xpld" to create a sam_e70_xpld.X folder.
This must be a valid directory name for your operating system.
- Name: Enter the project’s logical name as "getting_started_drivers_middleware_same70_xplained". This is the name that will be shown from within the MPLAB X IDE.
- Click Next to proceed to Configuration Settings.

Figure 5: Project name and location

Figure 6: MPLAB Harmony New Project Wizard Visual Help
Follow the steps below to set the project’s Configuration Settings.
Name: Enter the configuration name as "sam_e70_xpld".
- Target Device: Select ATSAME70Q21B as the target device.
- After selecting the target device, click Finish to launch MCC.

Figure 7: Configuration Settings
Open MCC and Configure Project Settings
While the MCC tool launches, click on Select MPLAB Harmony content type.

Click on the Finish Button in the MCC Content Manager Wizard.

Figure 8: MCC Launch
Set the created project as the main project. If you have multiple projects open, Right click on the project name, getting_started_drivers_middleware_same70_xplained, and click on Set as Main Project.

Figure 9: Set as Main Project
Open the Project Properties window by clicking on File and select Project Properties (getting_started_drivers_middleware_same70_xplained).

Figure 10: Open Project Properties
Verify that the compiler is set to XC32 (v4.30) and the Tool is set to SAM E70 Xplained (EDBG). You need to connect the tool using the DEBUG USB port on the SAME70 Xplained Evaluation Kit to your PC for this option to be visible. Also, verify the package version numbers.

Figure 11: Configure Project Properties