Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Miscellaneous Tab under the Options window of the Tools Menu in the MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:31
Miscellaneous Tab
The Miscellaneous category contains settings for features that don't fit under any of the other categories.
CSS Preprocessor
The CSS Preprocessors tab allows you to install and manage the Sass and LESS CSS preprocessors.
Diff
The Diff tab of the Miscellaneous category contains settings for the built-in diff utility as well as a means to launch an external diff tool instead.
The Diff tab in the Fonts & Colors category contains additional diff-related settings.
Files
The Files tab of the Miscellaneous category contains settings for file extension management.
File Associations
Default extensions are already set to be associated with each language tool. You can add or remove them here.
Files Ignored by the IDE
Regular expression describing files to be ignored.
Output
The Output tab allows you to set the font, font size, and message colors for the Output window.
Terminal
The Terminal tab of the Miscellaneous category contains settings that are a hold-over from Oracle's NetBeans Integrated Development Environment (IDE), upon which MPLAB® X IDE is based. These settings have no effect in MPLAB X IDE.
The Terminal window was a convenience for running command line programs for PC development. Its entry in the Window menu has been removed from MPLAB X IDE.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.