Starting an MPLAB® X IDE Debug Session
Last modified by Microchip on 2024/06/24 06:30
The Debug Project Icon
After ensuring the desired debug startup option has been set and ensuring the desired debugging tool has been selected, you can start a debug session by clicking on the Debug Project icon.
![]()
When a debug session has been initiated:
- The project will build.
- MPLAB® X Integrated Development Environment (IDE) will connect to the selected debug tool and download the built image.
- The Debug Icons will appear on the Toolbar.
- The application in the device will run according to the debug startup option.
This example shows the operation when the Debug Startup option is set to Halt at main.