Productivity Tools in the MPLAB® X IDE Editor
MPLAB® X IDE Action Items
The Action Items feature provides a convenient means to tag comments in your programs for special attention such as a "To Do" or "Fix Me" reminder. All comments that are tagged with one of the words or character patterns from the following table will be added to the Action Items window the next time the file or project is saved. Once a tagged comment is listed in the window, you can double-click on it and you will be taken immediately to its source in the Editor window.
How to Tag a Comment for Inclusion in the Action Items list
To tag a comment, simply use one of the words or character patterns from the table (or others you add to the list yourself) as the initial text of the comment. For example, to tag a comment with "TODO" you could use the following:
|TODO
|FIXME
|XXX
|PENDING
|<<<<<<
How to Add, Edit, or Remove Action Items Tags
From the main menu, select Tools > Options
In the window that opens, click on Team.

Select the Action Items tab.
Use the Add, Edit and Remove buttons on the right to modify the list to suit your needs.

How to Display the Action Items List
Select Window > Action Items from the main menu.
The Action Items window should appear as a tab below the editor near the Output tab.
Action Items comments in your code will not be added to the window until you save the project.

How to Add an Action Item to the List
Somewhere in one of your project's C source files, add a comment that starts like this:
Save the project by clicking on the Save All icon on the main toolbar. This will force IDE to parse all of the files. The TODO comment should now appear in the Action Items list.
Diff Utility
The Diff utility in MPLAB X IDE compares two files and displays the results in textual and graphical views. The following will explain how to access the Diff Utility, how to view Diff utility results, and other features offered by MPLAB X Diff utility.
Accessing Diff Utility
To access the Diff utility to compare two files, complete the following steps:
From the Project tree, double-click on the file name that you want to compare with, which will open the file in the Editor window.
In the MPLAB X IDE menu, go to Tools > Diff. This will open up a pop-up box with the title "Diff Filename To…".

Select the second file that you wish to compare with the first and click Diff.
By default, this will generate the graphical two-paned Diff viewer that displays the two files side-by-side with the differences highlighted.
You can also select the Textual View mode by clicking on the Textual tab.
Graphical View
Some of the highlights of this view are:
- The differences in the two files are highlighted with color code.
- Blue for actual differences.
- Green where blank spaces are not ignored.
- Pink where changes in inner white spaces are not ignored.
- The total number of differences is indicated at the top of the page.
- The center arrows indicate locations of differences.
- If you click on the center arrow, the file on the right side will instantly update with the corresponding contents in the file from the left side.

Textual View
The textual view displays the differences in a text format. The textual format is useful when the Diff file is to be shared with other users. MPLAB X IDE can use the textual Diff file and modify a file with the Diff file instantly.

Diff Viewer Menu
The Graphical and Textual Viewer also has an additional menu as shown below.

Diff Viewer Options
Additional options in the Diff view include the setting if the user wants to use the internal Diff utility provided in the MPLAB X IDE or use external Diff tool such as Windiff®.
Under the Internal Diff setting, you can also set the option to not use white spaces/changes within white spaces or case changes during Diff. The Diff results with these options selected are marked with color code as mentioned above.
The options menu can also be accessed within the MPLAB X IDE menu by navigating to Tools > Options > Diff tab.

Generate Doxygen Documentation
Open the Tools - Plugin Dialog
In the Plugins Available Plugins tab. Select Doxygen Integrator by checking the plugin in the plugin list.
Press the Install button and Select Next on the Plugin Installer Wizard.
Accept the License Agreement and install.
Select Restart Later and press Finish.

Download the Doxygen Executable from the link and install.
Restart MPLABX and select Tools - Options - Plugins tab.
Select the Doxygen Binary location.
Select or create a Doxygen Configuration file.
Select the Output path for the generated Doxygen documentation files per project.

Create Doxygen Documentation for Project
In the Projects Window right click on the logical folder project.
Select Create Doxygen from the context menu.
Output window tab for Doxygen Integrator opens with status of Doxygen document generation.
Select Doxygen HTML Output View
Additional Doxygen documentation.
You should now see the folder(s) you selected as logical subfolders in the Projects Window. Inside the folder are all the files it contained.
If the original folder on the hard drive contained subfolders, those will be added as logical subfolders as well. If they don't contain any files you need for the project, it is safe to remove them from the project.