Perform a Rectangular Edit in the MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:31
Since version 3.0 and later, the editor in MPLAB® X IDE can perform rectangular selections and edits. This comes in handy when working with blocks of data. As an example, consider the array defined below:
Let's say you want to replace the "8,9" at the end of all the rows with "3,4". With rectangular editing, you can easily replace the section as follows:
Click on the Toggle Rectangular Selection icon
in the editor toolbar.
Select the region you wish to copy.
Type Ctrl+C to copy the data.
Select the data that you want to replace.
Type Ctrl+V to paste and you will end up with: