Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Add Folder To Project in MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:34
Open the Add Folder Dialog
In the Projects Window, right click on thelogical folder where you want to add a new logical subfolder containing the new files. Select Add Existing Items from Folders… from the popup menu.
Click image to enlarge.
Open Dialog to Select Folder
Click on the Add Folder… button.
Click image to enlarge.
Select Folder
Select a folder that contains files you want to add to the project. The folder need not reside in the project's directory. You can navigate to other directories if necessary.
Click image to enlarge.
Add Folder(s) To Project
After selecting all the folders you want to add to the project, click the Add button.
Click image to enlarge.
You should now see the folder(s) you selected as logical subfolders in the Projects Window.
Inside the folder are all the files it contains.
If the original folder on the hard drive contained subfolders, those will be added as logical subfolders as well. If they don't contain any files you need for the project, it is safe to remove them from the project.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.