Code Profiler Plugin for the MPLAB® X IDE
Overview
This plugin for MPLAB® X IDE works with the MPLAB REAL ICE™ In-Circuit Emulator to display time-stamped function profiling of running project code, enhancing the software debugging capabilities of MPLAB X IDE.
It is used to measure the percentage of time spent in each function in order to determine where your application may be spending the greatest portion of time over an average collected set of data. It adds pre- and post-amble code to all functions in debug sessions and is available for most devices having data capture. It aids in debugging and code optimization by tracking the number of function calls, parent functions, child functions and execution time. Each license is intended for one user.
The use of this plugin requires an MPLAB REAL ICE In-Circuit Emulator.
The Code Profiling plugin supports these device families:
- PIC18F with data capture
- PIC24F, PIC24EP
- dsPIC33FJ, dsPIC33E
- PIC32MX with data capture
To find out if your device has data capture, please see the online Development Tool Selector.
The Code Profiling plugin DOES NOT SUPPORT these device families:
- PIC16F1
- PIC32MZ
These devices use a different type of data capture not supported by the plugin.
Code Profiling Capabilities and Limitations
The Code Profiling plugin displays:
- The number of calls to each function
- The percentage of time spent in each function
- The amount of time used by each function.
The percentage of time spent in each function and the number of calls to a function are reliably extracted. The user should not rely on the reported amount of time spent in each function as a definitive indicator of system performance. Code Profiling is a modestly "intrusive" process that prevents the precise timing information from being displayed. Code profiling's intrusion, however, can be measured and accounted for.
Code profiling is accomplished by "instrumenting" each function within the target code. This instrumentation process involves inserting a call at the beginning of each function that retrieves the PC and sends that data up through the debug tool to the IDE for time stamping and logging. Instrumentation also inserts a call at the end of each function that logs the corresponding function exit indicator. These calls add time to the function and may slow down system performance while profile data is being extracted. The amount of time added by these instrumentation calls depends upon the system clock speed, the MCU being used, and the compiler.
Timing with a Baseline Function
To determine the instrumented call overhead for a particular MCU/compiler/clock-speed the user will need to create and profile a baseline function. The baseline function is a function with little or no function overhead. A typical baseline function could be:
{
return;
}
When profiled, the measured execution time for a baseline function is the overhead for the instrumented calls for the current speed of MCU and compiler. By subtracting this number from time spent in each function the user will get a clearer view of the amount of time spent in each function.
Caveats for Baseline Function Timing
If the application being tested uses clock-switching to alter the speed of the system clock during execution, care should be taken on relying on the baseline function as a true overhead indicator as some functions may operate at different clock frequencies.
If a function under consideration makes calls in turn to other sub-functions, the instrumented overhead for these sub-calls would not be included in a simple baseline extraction analysis. Further analysis would need to be performed.
Requirements for Code Profiling
To perform code profiling you will need the following:
- MPLAB X IDE version 2.26 or higher with the Code Profiling plugin (SW100100) installed
- One of the following Microchip C compilers:
- XC8 (v1.20 or higher)
- XC16 (v1.20 or higher)
- XC32 (v1.20 or higher)
- MPLAB® REAL ICE™ in-circuit emulator
- One of the following PIC® Microcontroller (MCU) family members:
- PIC18F with Debug Data Capture
- PIC24FJ
- PIC24EP
- dsPIC33FJ
- dsPIC33E
- PIC32MX with Debug Data Capture
Not all PIC® MCUs can be profiled using the plugin. In order to work with the Code Profiling plugin the MCU must be able to allow the emulator to perform data capture during a debug session.
Verifying Debug Data Capture capability on the PIC® MCU
Open the Development Tools Selector - DTS.
Enter the Part Number in the Search Box
Select the "Emulators and Debuggers" tab
Look for the Words "Data capture: Enabled" under the REAL ICE™ section
Code Profiling Plug-in Installation
A trial version of the Code Profiling plugin can be installed from within MPLAB®X IDE. The Code Profiling Trial Version is a full-featured, 30-day time-limited version of the plugin.
The full-featured version of the plugin is available from Microchip Direct.
It is not necessary to install the trial version in order to get the full-featured version. The full-featured plugin can be downloaded and installed without previously installing a trial version.
Installing the Trial Version the Code Profiling Plugin
To begin the installation process, from the IDE window go to the Plugins menu under Tools
From the Available Plugins tab select Code Profiling (Trial Version), then select Install.
The Plug-in installer will launch the process in which the user will be asked to accept the license terms for the plugin. The installer will then download the most recent version of the plugin for installation.
At the end of the plugin installation process, the installer will prompt the user to restart MPLAB X IDE to make code profiling available.
Obtaining and Installing the full-featured Code Profiling Plugin
The Code Profiling Plugin (SW100100) is available on the "MPLAB® Xpress Cloud-Based IDE" page.
The plugin is delivered as two separately zipped .nbm files. Both of these files must be unzipped and installed for the plugin to operate.
To install:
Click the Install button and follow the instructions to finish the installation
Code Profiling Plug-in Setup
Setting the MCU Speed:
Click Apply.
Enabling Function Level Profiling
From the Project Properties Window:
Check Include Time Stamp. Two files are produced:
- a file containing raw polling and time stamp data (the log file)
- a file containing information about the log file, i.e., how to interpret the log file's contents (the .INX file)
Click OK.
Starting the Code Profiler
To collect data and time stamp information for profiling:
![debug project button](/xwiki/wiki/graphics/download/mplabx/ide/toolbar/project/debug-project.png?rev=1.1)
![continue button](/xwiki/wiki/graphics/download/mplabx/ide/toolbar/debug/continue.png?rev=1.1)
![pause button](/xwiki/wiki/graphics/download/mplabx/ide/toolbar/debug/pause.png?rev=1.1)
![line button](/xwiki/wiki/graphics/download/mplabx/ide/window/debugging/breakpoints/line.png?rev=1.1)
Code Profiling Window
The Code Profiling window displays function-level instrumentation counts, with timing, for each function entry and return during a sampled interval.
At the top of the Code Profiling window are totals:
- Time Stamps - Count of every function entry and return sampled during execution
- Calls - Count of every function entry sampled during execution
- Time - Duration of sampling (mS)
The data in the Function Time tab shows three sets of data for each function:
- Calls to Function
- Excluded Times
- Included Times
Calls to Function
There are two columns in the Calls to Functions data set (shown in pink in the Code Profiling window).
The Calls column displays the number of times the function in the Function column was called during execution.
The Percentage column shows the percentage of the total functions calls were made to the function named in the Function column.
Excluded Times
There are four columns in the Excluded Times data set (shown in green in the Code Profiling window).
The Excluded (mS) is the time spent in the function listed in the Function column, excluding the time used by the functions called by the named function.
Example of Excluded Time
If Function F1 calls Function F2 which in turn calls Function F3 the figure below shows the excluded time.
The “Avg (mS)” column displays the average excluded time for each call to the function.
The “Min-Max (mS)” column shows the slowest and fastest excluded times for the function.
The "Percentage” column shows the percent of the total excluded profile time used by each function time.
Included Times
There are four columns in "Included Times" data set (shown in blue in the Code Profiling window).
The “Included (mS)” column is the time spent in the function listed in the “Function” column including the time spent by functions called.
Example of Included Time
If Functions F1 calls Function F2 which in turn calls Function F3 the figure below would represent the Included Time.
The Avg (mS) column displays the average duration of the included function times.
The Min-Max (mS) column shows the shortest and longest included amount of included time for each function.
The Percentage column display the percent of the total included profile time represented by each function time.
Graphing Profile Data
To display the Code Profiling data click on the Display Timeline Graph button .
The Code Profiling Graph Window will appear displaying the time spent in each function for the entire simulation period.
The X-axis Time (mS) shows the profile time (in milliseconds) for the entire sample session
The Y-axis - Duration ms shows the time spent in each instance of a function call. The functions are color coded in the graph with the legend at the bottom of the graph
Panning
To move left and right through the data on the Time axis, use:
- The Pan Graph slider
- <Ctrl> + click on mouse (on Windows and Linux OS systems)
- <Apple> + click on the mouse (on Mac OS systems)
Zooming
Ensure the magnifying glass icon is selected:
- Click and drag with your mouse to zoom in.
- Right click on the graph, click on Zoom In or Zoom Out, and select an axes on which to zoom.
- Use the mouse wheel to zoom on the Time axis and <Ctrl> + mouse wheel to zoom on the Duration axis.
Reset the Zoom by clicking Reset Zoom.
Data Point Values
The graph allows the user the ability to specific time intervals manually. To do this first ensure magnifying glass icon is NOT selected then click and drag with the mouse to measure a time interval.
Code Profiling Controls
The Code Profiling Plugin has control icons and associated windows to assist in data display and analysis.
- Code Profiling Window
- Code Profiling Graph Window
- Chart Properties Window
Code Profiling Window Controls
The Code Profiling window opens up next to the Output tab in the IDE when the plugin is run. It has several control icons, all but one of the icons is on the left side of the window. The Column Setup icon is on the right side of the window.
Code Profiling Window Icons
Icon | Text | Description |
![]() | Project Properties | Open the Project Properties window. |
![]() | Filter Functions | Filter the display to show only the selected functions. Note: Code is not run again, the data already collected is reduced to remove all non-selected functions. |
![]() | Filter Select All | Select to display all functions. |
![]() | Show Function Timeline Graph | Display a graph of data in the window. |
![]() | Output Statistics | Output window data to a file. |
![]() | Column Setup | Click to display a menu for selecting which columns to show or hide. Also, show or hide horizontal scroll or pack columns (all or selected). |
The Code Profiling window has a context menu. The context menu items may be accessed by right-clicking anywhere in the Code Profile window.
Code Profiling Window Context Menu
Item | Description |
Clear View and Data | Clear all function data from the window. |
Reload Data | Reload function data from a file into the window. |
Code Profiling Graph Window
The Show Function Timeline Graph button can be found on the left side of the Code Profile window. Clicking on this icon opens up a graph of the simulation timeline.
Code Profiling Graph Window Icons
Icon | Text | Description |
![]() | Measure/Zoom mode select | Icon unselected: Measurement mode. Drag mouse to measure time value. Icon selected: Zoom mode. Drag mouse to zoom in on an area. |
The Code Profiling Graph window has a context menu. To access the context menu, right-click anywhere inside the Graph window.
Code Profiling Graph Window Context Menu
Item | Description |
Turn Off/On Zoom mode | Click to disable Zoom mode. Click again to enable Zoom mode. |
Save graph image | Save an image of the graph to a PNG file. |
Print the graph. | |
Zoom In | Zoom in on graph data. Choose to zoom in on: - Both Axes - Domain Axis (x coordinates) - Range Axis (y coordinates) |
Zoom Out | Zoom out on graph data. Choose to zoom in on: - Both Axes - Domain Axis (x coordinates) - Range Axis (y coordinates) |
Zoom Reset | Reset zoom to default level. |
Properties | Open the Chart Properties window. |
When Properties is selected from the Graph window, the properties window appears. This window has four tabs: Tile, Plot, Appearance, and Other. The table below shows the functions found under these tabs.
Chart Properties Window
Set up the graph look and feel on the tabs of this window.
Title Tab
Item | Description |
Show title | Check to show the graph title listed under Text. Uncheck to hide the graph title. |
Text | Enter a title for the graph. Show Title must be checked. |
Font | Select font options for the graph title text. |
Color | Select a color scheme for the graph title text. |
Plot Tab
Item | Description |
Label | Enter a label for the axis. |
Font | Select font options for the label. |
Paint | Select a color scheme for the label (text and background). |
Ticks | Check to show tick labels. Uncheck to hide. Select font options for the tick labels. Check to show tick marks. Uncheck to hide. |
Range | Check to auto-adjust range values. Uncheck to enter a minimum range value and a maximum range value. |
TickUnit | Check for Auto-Selection of TickUnit. Uncheck to enter TickUnit value. |
Appearance Tab
Item | Description |
Outline stroke | Select the thickness of the line around the graph. |
Outline paint | Select the color of the line around the graph. |
Background paint | Select the color of the graph background. |
Orientation | Select an orientation for the graph domain ![]() - Vertical (default) - Horizontal |
Other Tab
Item | Description |
Draw anti-aliased | Check to use anti-aliasing when drawing the graph. Uncheck to turn anti-aliasing off. |
Background paint | Select the color of the background outside of the graph. |
Series pain | Not implemented. |
Series stroke | Not implemented. |
Series outline paint | Not implemented. |
Series output stroke | Not implemented. |