Converting An MPLAB® 8 IDE Project to the MPLAB X IDE
Overview
If you have a project from in the MPLAB® 8 IDE, in most cases it can easily be converted to the new MPLAB X IDE format. There are however a few things you can do first to help ensure that the process goes smoothly.
- From time to time, the project file format of MPLAB 8.x and earlier has changed. To ensure that you are using the latest project file format before attempting the conversion, first, save your project with MPLAB 8.14.03A or later.
- If your project #includes files that are not in the project tree (other than those that are installed with the compiler or assembler), include them in the header folder of the project tree so that the conversion utility can find them. (Required for beta versions of MPLAB X IDE)
- If your project uses relative paths for its files, ensure that all required files are still present in their relative locations.
Also, if you are planning on running MPLAB X IDE on Linux® or a Mac®, there are a couple of other items you need to consider:
- Linux and Mac file systems are case-sensitive. Header file names must match the case of the actual files. For example: #include "p24fj128ga010.h" will not work. The file will not be found because the actual file name is p24FJ128GA010.h, where all letters except the initial 'p' and final 'h' are capitalized.
- Relative paths must use forward slashes '/' which work on all operating systems rather than back slashes '\' which work only on Windows. For example, #include "Graphics\Graphics.h" needs to be changed to #include "Graphics/Graphics.h".
Step-by-Step Tutorial
Open the New Project Wizard
From the menu, select File ► New Project… or click on the New Project icon
on the toolbar.
Choose Project Type
From the Categories list, choose Microchip Embedded and from the Projects list, choose Existing MPLAB IDE v8 Project. Click Next > when done.
Click image to enlarge.
Locate MPLAB 8 .mcp File
Click the Browse… button and select the *.mcp file for the project you wish to convert. Click Next > when done.
Click image to enlarge.
Select Device and Header
The project's target device should be automatically detected from the *.mcp file, so just click Next >. You may however change to a different device if you know the older project supports it. After hitting next, IF your device requires a debug header you will be prompted to select the header. If the device you are using does not require a debug header you will proceed to Tool Selection.
A header interface provides debug capability with no pin loss to the target application. Headers are required for most low pin-count devices and are available as an option for some high pin-count devices.
An example of a low pin-count device's header is shown below.

- If you are using a debug header, check the box. Otherwise, leave it unchecked.
- Click Next >
Click image to enlarge.
Select Tool
Choose the debug/programming tool you wish to use with the new project. Click Next > when done.
Click image to enlarge.
Select Compiler
Choose the compiler or assembler you wish to use with the new project. Click Next > when done.
Click image to enlarge.
Select Project Name and Folder
By default, the MPLAB X IDE project directory will be created inside the MPLAB 8 project's directory. Here, you can change the location and/or name of the new project and its directory. Click Next > when done
Click image to enlarge.
Summary
This slide simply shows you what the converter will do and where it will do it. Click Finish when done.
Click image to enlarge.
Your project has now been converted. You should see all of the files from the MPLAB 8 project tree in the new MPLAB X IDE project tree. You should now be able to successfully build your project by clicking the build button
on the toolbar without any further changes. If you get any messages about a compiler not being found you may need to configure your compiler for MPLAB X IDE.