Create a Prebuilt Project (HEX File) in MPLAB® X IDE
Overview
Because MPLAB® X IDE is project-based, it is not possible to simply import a HEX file as was done in MPLAB 8. However, the same result may be achieved by creating a pre-built project. This will create a project "wrapper" around the HEX file so that it may be used the same way as a HEX file built from within a project. The main difference is that you will be able to program a target without being required to build the project since the HEX file already exists.
Procedure
Launch New Project Wizard
Launch the New Project Wizard by using one of the following methods:
- Toolbar:

- Keyboard: CTRL + SHIFT + N
- Menu: File > New Project...
Select Project Type
- Select Microchip Embedded from the Categories list.
- Select Prebuilt (Loadable Image) Project from the Projects list.
- Click Next >
Click image to enlarge.
Select File, Device, and Tool
- Click the Browse button, locate, and select the Prebuilt .hex file from your computer.
- Select your microcontroller from the Device drop drop-down.
- Finally, select the Hardware Tool you will use to program the microcontroller.
- Click Next >
Click image to enlarge.
Select Project Name and Folder
- Select a Project Name for your project.
- Select the Project Location on your computer.
- Click Finish>
Once you click Finish the project has been created. It will now be open in the project tree.
Click image to enlarge.