Hex Files in MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:33
Creating A Production Hex File
| To build a production image, click on one of the following icons within MPLAB® X IDE |
| Name | Description | |||
![]() | Clean and Build Project | Deletes all the intermediate files, then re-compiles all source files in the project. After compilation, all the newly created intermediate files are linked together to create a single image file. | ||
![]() | Build Project | Sometime referred to as 'make'. Re-compiles only the files which have changed since the last build. Unchanged intermediate files are kept. After compilation, a single image file is created by linking the intermediate files. | ||
![]() | Make and Program Main project | This icon has two actions: the first is to invoke the Build Project function and the second is when the project is built, the image is downloaded to the PIC® MCU through the selected hardware tool for the project. | ||
- The production HEX file is placed within the dist subdirectory of the project folder. The exact subdirectory depends upon which MPLAB X project configuration is used. When no configuration is specified, MPLAB X uses a default subdirectory called default. Within the dist\<configuration> directory, the HEX file will be found in the production subdirectory.
- Once the project is built, the HEX file for a project is created using the project name formatted as ProjectName.X. If the default configuration is used, it may be found at the following location:


Read a Device and Save the Hex File
From the main toolbar, click on the small downward pointing triangle on the right edge of the Read Device button. A drop down menu will appear. Select Read Device Memory to File…. You will be prompted for a location to save the hex file.