Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Allocating Heap Memory in MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:34
Heap A contiguous block of memory can be set aside to be used as a "scratch pad" by the application program at run-time. Many applications and functions require the use of a heap. When a heap is required the developer must configure the heap inside the MPLAB® IDE X project.
Care should be taken when creating a heap. Memory used in the heap is unavailable for global variables or the stack. Making a heap larger than it needs to be may make it difficult for the linker to complete the memory allocation.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.