Window Groups and Accessing New Windows in the MPLAB® X IDE
Window Groups
To simplify the interface appearance, MPLAB® X IDE displays each window as a tab inside of a window group. By default, MPLAB X IDE provides four window groups: Project, Editor, Navigation, and Output.

Default Window Groups
Project Group
- Projects
- Files
- Favorites
- Tasks
- Classes
- Services
Editor Group
- Editor
- Disassembly
- Data Visualizer
- Power Monitor
- Kit Window
- Programming Center
- Start Page
- MPLAB Store
Navigation Group
- Dashboard
- Navigation Window
Output Group
- Output
- Debugging Windows
- Variables
- Watches
- Call Stack
- Breakpoints
- Sessions
- Sources
- Target Memory Views
- Program Memory
- File Registers
- SFRs (Special Function Registers)
- Configuration Bits
- User ID Memory
- IO View
- AppIO
- Simulator
- Stimulus
- Logic Analyzer
- IOPin
- RegisterTrace
- Bookmark
- Terminal
Accessing Additional Windows
Depending on the revision, and the plugins installed, MPLAB X Integrated Development Environment (IDE) can provide the user with more than 30 interface windows. These windows allow the user to enter data and control, or observe, certain aspects of application development.
As the user progresses through the development process, the IDE will open the appropriate windows. For example, when a source file is opened, the IDE will open the Editor window allowing the user to change the contents of the file. When a project is built, MPLAB X IDE opens the Output window to display the status of the build.
Windows can also be accessed through the Window Menu (as shown in the accompanying image).