MPLAB® IPE Environment Settings
Last modified by Microchip on 2023/11/10 11:02
Environment Settings
Environments allow you to save settings so that the same settings can be reloaded in another programming session. Environments are supported, under all tools, as either PEN files or PM3 files.
To view and change the Environments options, you need to first log in to the Advanced Mode and then click on Environment to display the available settings.

The Environment options table provides a brief description of the Environment options settings.
Environment Options
| Setting | Description |
|---|---|
| Environment Name | The environment name you specify |
| .pm3 file | For MPLAB® PM3 Universal Device Programmer, select this type of file |
| .pen file | For MPLAB ICD 3 In-Circuit Debugger, MPLAB PICkit™ 4 Debugger/Programmer, and MPLAB REAL ICE™ In-Circuit Emulator tools, select this type of file |
| Description | The description you use for the environment |
| SQTP(SM) File | The SQTP file name used in the environment |
| Misc Files | Other files used in the environment, e.g., datasheets, instructions, etc. Multiple files can be selected |
| Properties | Click this button to display the properties of the SD card in the MPLAB PM3 Universal Device Programmer |
| Format | Click this button to format the SD card in the MPLAB PM3, erasing all of the contents |
| Delete | Opens the Delete Environment window |
| Copy | Opens a dialog to select source and destination for copying environment |
| View | Opens the View Environment window |
| Save to PM3 SD Card | Saves the files to an MPLAB PM3 SD card destination |
| Save to PC | Saves file to a destination on the PC |