SAM9X60-EK Evaluation Kit - Booting from QSPI Flash Memory
- Introduction
- Prerequisites
- Hardware
- SAM-BA In-System Programmer
- Erase QSPI Flash Memory
- Build at91bootstrap and Write to QSPI Flash Memory
- Build u-boot-at91 and Write to QSPI Flash Memory
- Create u-boot-env.bin and Write to QSPI Flash Memory
- Build the Linux Kernel Image and Device Tree Blob (DTB)
- Create a Flattened Image Tree
- Prepare a Root File System (ROOTFS) for SD Memory Card
- Write Image Tree Blob to SD Memory Card
- Boot from QSPI Flash Memory
- Summary
- What's Next?
Introduction
This training topic explains how to configure and program the SAM9X60-EK Evaluation Kit to boot the second- and third-stage bootloaders at91bootstrap and u-boot-at91 from Quad Serial Peripheral Interface (QSPI) Flash Memory, and the Flattened Image Tree (FIT) (containing the Linux® kernel and Device Tree) and Root File System from the SD memory card.
You will use the SAM-BA® In-System Programmer to write at91bootstrap and {u-boot-at91 to QSPI Flash memory.
Steps
- SAM-BA In-System Programmer
- Erase QSPI Flash memory
- Build at91bootstrap and write to QSPI Flash memory
- Build u-boot-at91 write to QSPI Flash memory
- Create u-boot-env.bin and write to QSPI Flash memory
- Build the Linux® kernel and Device Tree Blob (DTB)
- Create Flattened Image Tree and write to QSPI Flash
- Prepare a Root File System (ROOTFS) for SD memory card
- Write Image Tree Blob (ITB) to SD memory card
- Boot from QSPI Flash memory
Prerequisites
- Familiar with the features of the SAM9X60-EK evaluation kit
- A working cross-toolchain for Arm®-based MPU target
- Familiar with the operation of the SAM-BA In-System Programmer
- Setup Console Serial Communications for the SAM9X60-EK
- Knowledge of the Boot Process:
- SAM9X60 Boot Process
- SAM9X60 Datasheet (Section 12 – Boot Strategies)
Hardware

For this training topic, you will be using the SAM9X60-EK Evaluation Kit. You will also need two USB Micro-B cables. One cable will connect the Host PC to the target console to view the SAM-BA Monitor log message. The second cable will connect the Host PC to the target USBA port (J7) so that the SAM-BA Host can communicate with the SAM-BA Monitor.
Bootable Memory
For this training, you will use the Quad Serial I/O™ (QSPI) Flash memory (U8) (64 Mbit Quad Serial I/O Flash memory SST26VF064B to boot the second- and third-stage bootloaders, at91bootstrap and u-boot-at91.

As the QSPI Flash memory is not large enough to hold all the bootable images, you will boot the kernel image (linux_at91) and root filesystem (RootFS) from the SD memory card (J4).

SAM-BA In-System Programmer
In this section, you will load the SAM-BA Host Application (if you have not already done so) and set up Console and SAM-BA Host to Monitor communications.
Setup SAM9X60-EK Console Serial Communications
To view the SAM-BA Monitor log messages, set up console serial communications following the instructions in the topic: SAM9X60-EK Console Serial Communications.
You have two choices in connecting to a serial port on the SAM9X60-EK:
- The first is using a USB cable to connect to the J-LINK-OB port (J22). This method has the added benefit of powering the SAM9X60-EK.
- The second is using a USB-to-TTL converter to connect to the Universal Asynchronous Receiver Transmitter (UART) Debug port (J24). With this option, to power the SAM9X60-EK, you will need to:
- Use an external 5 VDC power supply connected to J1 (coaxial power jack), or:
- Use a USB cable connect to the USBA port (J7). As you’ll be connecting a USB cable in Step 3 below (SAM-BA Host to Monitor Communications), this is the easiest method.


If it is not already installed, install the SAM-BA Host Application.
Setup the SAM-BA Host to Monitor Serial Communications
a. To communicate with SAM-BA Monitor on the target, you must have installed the SAM-BA Host on a Linux PC (Step 2 above), and connect a USB Micro-B cable from the host PC to the USBA port (J7) on the SAM9X60-EK as shown in the accompanying figure.
b. Ensure there is no SD memory card inserted in slot J4.
c. Open the DISABLE_BOOT (J13) jumper.
This will allow booting from the onboard memories (NAND and QSPI Flash).
d. Press both the DIS_BOOT (SW4) and RESET (SW3) push buttons.
Pressing the DIS_BOOT (SW4) push button disables booting from the onboard memories.
e. Continue pressing DIS_BOOT(SW4) while releasing the RESET (SW3) push button.
The SAM9X60-EK will boot to the SAM-BA Monitor and start communications with the SAM-BA Host. Observe ROMBoot on the Console (terminal emulator) indicating the SAM-BA Monitor is running.
Erase QSPI Flash Memory
In this section, you will erase the contents of the QSPI Flash memory located on the SAM9X60-EK. This is a necessary step before writing data to the QSPI Flash memory.
Erase QSPI Flash Memory
Erase the contents of the QSPI Flash memory on the SAM9X60-EK with the following command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 8388608 bytes.
Page size is 256 bytes.
Buffer is 112644 bytes (44 pages) at address 0x0030a3e0.
Supported erase block size: 4K
Executing command 'erase'
Erased 4096 bytes at address 0x00000000 (0.05%)
Erased 4096 bytes at address 0x00010000 (0.10%)
..
..
Erased 4096 bytes at address 0x003e0000 (99.95%)
Erased 4096 bytes at address 0x003f0000 (100.00%)
Connection closed.
Build at91bootstrap and Write to QSPI Flash Memory
In this section, you will configure and build the second-stage bootloader, at91bootstrap, from source code to boot from QSPI Flash memory and write it to QSPI Flash memory.
Change directory into the at91bootstrap directory:
Using a default configuration file, configure at91bootstrap to boot u-boot from QSPI Flash memory:
# CLEAN obj and miss files!
# CLEAN configuration files!
# CLEAN binary files!
$ make sam9x60ekdf_qspi_uboot_defconfig
#
# configuration written to .config
#
#
# make dependencies written to .auto.deps
# See top of this file before playing with these auto-prerequisites!
#
Optional: If you would like to verify the QSPI Flash memory settings or make any customizations:

a. Observe that Board Type (sam9X60ek) has been selected.
b. Highlight Memory selection ---> and press ENTER.
c. Highlight QSPI flash configuration ---> and press ENTER.
You can see QSPI Bus Select is QSPI Bus 0.
You may exit menuconfig by repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build at91bootstrap:
Once the build is complete, the resulting binary files are in the /at91bootstrap/binaries/ directory:
$ ls
at91bootstrap.bin
boot.bin
sam9x60ek-dataflashboot—uboot-3.9.2.bin
sam9x60ek-dataflashboot-uboot—3.9.2.elf
sam9x60ek-dataflashboot-uboot—3.9.2.map
From the SAM-BA Host command line, write at91bootstrap.bin to QSPI Flash memory starting at location 0x0 using the qspiflash applet writeboot command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 8388608 bytes.
Page size is 256 bytes.
Buffer is 112644 bytes (44 pages) at address 0x0030a3e0.
Supported erase block sizes: 4K
Executing command 'writeboot:at91bootstrap.bin'
Appending 8 bytes of padding to fill the last written page
Wrote 11264 bytes at address 0x00000000 (65.676%)
Wrote 5888 bytes at address 0x00002c00 (100%)
Connection closed.
The result is at91bootstrap.bin is stored in the QSPI Flash Memory starting at address 0x0.
Build u-boot-at91 and Write to QSPI Flash Memory
In this section, you will configure and build the third-stage bootloader, u-boot-at91, from source code to boot from QSPI Flash memory and write it to QSPI Flash memory.
Change the directory to your working directory containing the u-boot-at91:
Using a default configuration file, configure u-boot-at91 for QSPI Flash memory:
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/zconf.tab.o
HOSTLD scripts/kconfig/conf
#
# configuration written .config
#
Optional: If you would like to verify settings for booting from QSPI Flash memory or make any customizations, type:

a. Highlight Boot media ---> and press ENTER.
b. Observe that [*] Support for booting from QSPI flash ---> has been selected.
You may exit menuconfig by repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build u-boot-at91:
Once the build is complete, the resulting binary file u-boot.bin is in the u-boot-at91 directory.
From the SAM-BA Host command line, write u-boot.bin to QSPI Flash memory starting at location 0x40000 using the applet -a qspiflash -c write command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 8388608 bytes.
Page size is 256 bytes.
Buffer is 112644 bytes (44 pages) at address 0x0030a3e0.
Supported erase block sizes: 4K
Executing command 'write:u-boot.bin:0x40000'
Appending 210 bytes of padding to fill the last written page
Wrote 11264 bytes at address 0x00040000 (1.87%)
Wrote 11264 bytes at address 0x00042c00 (3.73%)
…
…
Wrote 11264 bytes at address 0x000cf000 (98.86%)
Wrote 11264 bytes at address 0x00d1cc00 (100.00%)
Connection closed.
The result is u-boot.bin is stored on the QSPI Flash memory starting at address 0x40000.

Create u-boot-env.bin and Write to QSPI Flash Memory
Configuration of U-Boot is performed using environment variables. They are stored in binary format, generally, on the same boot memory (mass storage) that U-Boot is stored.
In this section, you will create a U-Boot environment binary file by first creating a text file. The text file is then converted to binary format using a utility program mkenvimage. Finally, you will write the file to QSPI Flash memory using the SAM-BA In-System Programmer (ISP).
Using your favorite text editor, create a text file with the following information. Name the text file u-boot-env.txt.
bootcmd=ext4load mmc 0:2 0x24000000 boot/sam9x60ek.itb; bootm 0x24000000#kernel_dtb
bootdelay=1
ethact=gmac0
stderr=serial
stdin=serial
stdout=serial
The bootargs line tells U-Boot:
- The console device and baud
- The root= location of the root filesystem and permissions
- The rootfstype= root filesystem type
The bootcmd= line tells U-Boot to load the sam9x60ek.itb file (Flattened Image Tree (FIT)) from the EXT4 formatted partition 2 on the SD Memory Card (which you will prepare in future sections) to external DDR2 SDRAM starting at address 0x24000000.

Convert the text file u-boot-env.txt into a binary file u-boot-env.bin using the utility program mkenvimage.
From the SAM-BA Host command line, write u-boot-env.bin to QSPI Flash memory starting at location 0x140000 using the applet -a qspiflash -c write command:
Opening serial port 'ttyACM0'
Connection opened.
Detected memory size is 8388608 bytes.
Page size is 256 bytes.
Buffer is 112644 bytes (44 pages) at address 0x0030a3e0.
Supported erase block sizes: 4K
Executing command 'write:u-boot-env.bin:0x140000'
Appending 210 bytes of padding to fill the last written page
Wrote 11264 bytes at address 0x00140000 (8.59%)
Wrote 11264 bytes at address 0x00142c00 (17.19%)
…
…
Wrote 11264 bytes at address 0x00015b800 (94.53%)
Wrote 11264 bytes at address 0x0015e400 (100.00%)
Connection closed.
The result is u-boot environment is stored in the QSPI Flash Memory starting at address 0x140000.

Build the Linux Kernel Image and Device Tree Blob (DTB)
In this section, you will configure the Linux kernel and device tree for the SAM9X60-EK Evaluation Kit using the default configuration and build the files. In the next section, you will use these files to create a Flattened Image Tree image and write it to the SD memory card.
Change directory to your working directory containing the linux-at91 source code:
Using default configuration files, configure the Linux kernel using the following command:
HOSTCC scripts/basic/fixdep
HOSTCC scripts/kconfig/conf.o
HOSTCC scripts/kconfig/confdata.o
HOSTCC scripts/kconfig/expr.o
LEX scripts/kconfig/lexer.lex.c
YACC scripts/kconfig/parser.tab.[ch]
HOSTCC scripts/kconfig/lexer/lex.o
HOSTCC scripts/kconfig/parser.tab.o
HOSTCC scripts/kconfig/preprocess.o
HOSTCC scripts/kconfig/symbol.o
HOSTLD scripts/kconfig/conf
#
# configuration written to .config
Optional: If you would like to verify settings or make customization changes type:

You may exit menuconfigby repeatedly typing "ESC-ESC" until it closes. Do not save any changes.
Build linux-at91:
Once the build is complete, the resulting binary files are created:
/arch/arm/boot/dts/at91-sam9x60ek.dtb
Create a Flattened Image Tree
In this section, you will create a Flattened Image Tree (FIT). The FIT image allows for more flexibility in handling images of various types and enhances the integrity protection of images with stronger checksums. An Image Source (*.its) file and a set of data files are used as an input. An Image Tree Blob (*.itb) file is generated as the output. Finally, you will write the FIT image to the SD memory card.
Git clone the Device Tree Overlay files from the Linux4SAM repository:
Change the directory to your working directory containing the dt-overlay-at91:
Open Makefile with your favorite editor and verify that the KERNEL_DIR is pointing to your linux-at91 directory:
DTC_OPTIONS?=-@
DTC_OPTIONS += -Wno-unit_address_vs_reg -Wno-graph_child_address -Wno_pwms_property
KERNEL_DIR?=../linux-at91 <--- Ensure pointing to your linux-at91 directory
KERNEL_BUILD_DIR?=$(KERNEL_DIR)
DTC?=$(KERNEL_BUILD_DIR)/scripts/dtc/dtc
Or you can set the KERNEL_DIR environment variable:
$ echo $KERNEL_DIR
Build the *.itb image file:
Once the build is complete, the resulting image file sam9x60ek.itb is located in the dt-overlay-at91 directory.
Remember this directory location as you will be copying the sam9x60ek.itb image to the SD memory card.
In the next section, you will prepare an SD memory card.
Prepare a Root File System (ROOTFS) for SD Memory Card
In this section, you will download a demonstration image from the Linux4SAM website to use the Root File System on the image. You will Flash the image to an SD memory card and delete the files in the BOOT partition. Finally, you will copy the Flattened Image Tree file that you created in the previous section to the ROOTFS/boot directory.
Download SAM9X60-EK demonstration image from the Linux4SAM website.
There you will find three sets of images created from one of three Build Systems:
- The Yocto Project
- Buildroot
- OpenWRT
Any one of the images can be used for this step. If you are undecided, choose the linux4sam-buildroot-sam9x60ek-headless file.
Flash the demo image to an SD memory card.
Insert the SD memory card into a Linux desktop computer.
Delete the files in the BOOT(FAT32) partition.
Write Image Tree Blob to SD Memory Card
Copy the sam9x60ek.itb file to the ROOTFS/boot directory.
$ cp sam9x60ek.itb /media/<username>/ROOTFS/boot
Boot from QSPI Flash Memory
Check that you have Console Serial Communications established.
Review Step 1 of the SAM-BA In-System Programmer section above.
Check that jumper in the DIS_BOOT (J13) is open.
This will allow booting from the onboard memories (NAND and QSPI Flash).
Insert the SD memory card into J4.
Press the Reset button SW3 (nRST).
The boot log will display in the terminal emulator. In the end, the command line will prompt the user to log in. Login as root. There is no password required to login.
Proper operation of the image will be indicated by a flashing blue RGB LED (LD1).
If Console Serial Communications is connected to J22, the operation of the onboard J-Link Debugger will be indicated by a Flashing green LED (D9).
Congratulations! You have created an embedded Linux system that boots from QSPI Flash memory.
Summary
In this training topic, you configured and built the second-stage bootloader at91bootstap and the third-stage bootloader u-boot-at91 from source code. You wrote the second- and third-stage bootloaders into QSPI Flash memory. You also prepared an SD memory card with Flattened Image Tree (containing the Linux kernel and Device Tree) and Root File System. The result is an embedded Linux system that boots from QSPI Flash memory.
What's Next?
- SAM9X60-EK Evaluation Kit - Fast Boot Demonstration
- SAM9X60-EK Evaluation Kit - Booting from SD Memory Card
- SAM9X60-EK Evaluation Kit - Booting from NAND Flash Memory