SAM9X75 Curiosity Wireless Kit - Wi-Fi® Quick Start Guide for MPLAB® Harmony v3

Last modified by Microchip on 2026/01/09 08:12

Introduction

Thank you for evaluating the SAM9X75 Curiosity Wireless Kit. This guide will assist you in running the demonstration application designed for the kit. For a more detailed exploration of the kit's features and capabilities, please refer to the links in the "Explore Applications" section of this guide.

Pre-Requisites:

  • Confirm the following components are present out of the box:
    • SAM9X75 Curiosity Board 
    • LAN8840 EDS2 SODIMM extension board (P/N: EV12N54A)
    • RNBD451 Add-on Board (P/N EV25F14A)
    • WILCS02 M.2 Wi-Fi® Module Card (P/N EV59Y78A)
    • SD card
    • USB Type-A to Micro-USB cable (power)
  • Prepare the following hardware:
    • PC with an SD card reader and admin rights
    • Serial to USB dongle (FTDI)
  • Install the following applications on the Windows® PC

This quick start guide will help you enable the Soft Access Point (SoftAP) on the SAM9X75 Curiosity Wireless Kit, allowing a smartphone or PC to access a static web page through a browser over Wi-Fi.

Note the "Troubleshooting"  section at the bottom of this page for some more help.

MPLAB® Harmony v3 Hardware Setup

Program the WIxCS02 M.2 Wi-Fi Module with the correct firmware image.

Download the M2_Harmony_support.img file from the repository, GitHub EA03X56A-wifi/m2.

Back to Top


Copy the downloaded file into the SD memory card using balenaEtcher.

Insert the SD memory card into the PC.

Download, install, and run balenaEtcher.

Select the downloaded M2_harmony_support.img file.

balenaEtcher window Flash from File button

Click Select target to download.

balenaEtcher window Select target button

Select the mounted SD card.

balenaEtcher window Select 1 button

Select Flash.

balenaEtcher window Flash button

The SD card will be ready for use once flashing is completed.

Back to Top


Connect the components as shown in the accompanying images:

Insert the flange and antenna assembly into the antenna hole labeled FD1 .

Secure the antenna into the flange with the antenna wire going under the hole provided.

Secure the antenna into the flange Secure the antenna into the flange

Insert the WIxCS02 M.2 Wi-Fi Module into the J20 M.2 connector. 

Insert WIxCS02 M.2 Wi-Fi Module

Secure the provided screw on the tapped hole provided labeled as STANDOFF1.

Secure the provided screw

Insert the SD card in the SD Boot J14 slot.

Connect the serial-USB dongle to the UART DEBUG J35 header on one side and to the PC on the other side.

Set the J24:M.2 I/F SEL to SPI.

Connect the USB Type-A to Micro-USB cable to J2 Micro-​​​​USB port for power.

Connect components

Back to Top

Set Up and Start SAM9X75 Curiosity Board Serial Terminal

Set up the SAM9X75 Curiosity Board serial terminal on the PC.

On the PC, open a serial terminal with the following settings:

  • Baud Rate: 115200
  • Data: 8-bit
  • Parity: None
  • Stop: 1-bit
  • Flow Control: None

Open PuTTY.
PuTTY icon

Open Windows Device Manager to find out which COM port to use: plug and un-plug the Serial-USB dongle and check which COMxx port appears and disappears (COM10 will be used in this example).

Open PuTTY > Category > Connection > Serial and configure the parameters as shown in the accompanying image (adapt the COM port to your local setup).

putty serial

Come back to PuTTY > Category > Session and check that Connection type is Serial, then press Open.

Putty session

 

Back to Top

Verify M.2 Module Update

Power the board on.

Back to Top


Using the console, confirm that the image copied in Step 2 is used in the Device Firmware Update. 

Confirm Device Firmware Update Image

Back to Top

Prepare the Application Image

Re-use the SD card used in Step 2 to program the MPLAB® Harmony v3 application image. 

Back to Top


Download the harmony_application.img file from the repository, GitHub_EA03X56A-wifi.

Back to Top


As already done in Step 2, copy the harmony_application.img in the SD card.

Back to Top


Re-insert the SD card into the SD Boot J14 slot. 

Back to Top


Press the RESET (SW3) button on the SAM9X75 Curiosity Board to force a reset.

When the system is ready, the serial terminal that was set up earlier in this tutorial should show the application running. 

Verify that the SoftAP MPLAB Harmony v3 application is running and displaying [APP] : Wi-Fi  [AP] connect to ... on the terminal.​​​​​​

Soft AP Harmony application is running image

Information

Note: The password to use ("password") when connecting to the access point is also shown on the terminal.

Back to Top

Perform the Test

Perform the test to display the static web page.

On the PC, connect to the Wi-Fi access point using the network name microchip-SoftAP.
Connect to access point image

Warning

Ensure there is no active Ethernet connection running simultaneously, as this may prevent the demo page from displaying properly.

Enter "password" for the passphrase/password.

On the PC, open a browser, then connect to the access point and enter the address "http://192.168.1.1" as the URL.

connect to the access point using the address: http://192.168.1.1 image

 

Confirm on the browser that the following page is displayed.

Success expected image

Information

Terminal will show connection activities.Show connection activities image

Another way to test the Wi-Fi SoftAP is to use a smartphone. Connect to the access point using the network name, microchip-SoftAP.

Connect to Soft-AP using smart phone image

Warning

Ensure there is no active internet connection (e.g., 4G, 5G) running simultaneously, as this may prevent the demo page from displaying properly.

Enter "password" for the passphrase/password.

On the smartphone, open a browser, then connect to the access point and enter the address "http://192.168.1.1" as the URL.

browser connection to access point using the address: http://192.168.1.1 image

Confirm on the smartphone browser that the following page is displayed.

Smart phone connection success image

Information

Note: The terminal will show connection activities.Terminal showing connection activities image

Back to Top


Congratulations! Your SAM9X75 board running MPLAB Harmony v3 is now connected over Wi-Fi to your PC or smartphone.

What's next? See the following sections for more resources.

Back to Top

Explore Applications

Wireless Applications

Transparent Universal Asynchronous Receiver Transmitter (UART) communication between a smartphone and the SAM9X75 Curiosity Board using a Bluetooth® Low Energy (LE) connection (SAM9X75 Curiosity Wireless Kit - BLE Quick Start Guide for Linux®)

MPLAB Harmony Wireless SolutionsRepository containing the MPLAB Harmony v3 Wireless_wifi solutions
MPLAB Harmony Wireless System ServicesRepository containing MPLAB Harmony v3 Wireless system services for RNWF02/WINCS02 device

Ethernet Applications

iPerf networking test between host PC (as a TCP Client) on Microchip Curiosity Board (as a TCP Server) (SAM9X75 Curiosity LAN Kit - Quick Start Guide for MPLAB Harmony v3)

MPLAB Harmony v3 Solutions

MPLAB Discover Code ExamplesSAM9X75 Peripherals and Drivers code examples
Microchip Graphics SuiteSAM9X75 User's Guide for Microchip Graphics Suite (MGS) for Harmony
Linux Solutions

Linux solutions for SAM9X75

Explore Hardware

SAM9X75 Curiosity LAN KitThe SAM9X75 Curiosity Development Board, featuring the high-performance, ultra-low-power SAM9X75D2G MPU with an ARM926EJ-S CPU running up to 800 MHz and integrated 2 Gbit DDR3L memory, serves as the evaluation platform for the SAM9X7 Series MPU devices.

The RNBD451 Add-on Board is a cost-effective development platform for evaluating the RNBD451PE Bluetooth LE module, featuring compliance with the mikroBUS™ standard and an on-board MCP2200 USB-to-UART converter for immediate use without additional hardware.

LAN8840 EDS2 Daughter Card

The EV12N54A LAN8840 EDS2 PHY Daughter Card offers copper Gbit Ethernet connectivity for Microchip development platforms using the EDS2 interface, featuring the LAN8840 transceiver with PTP support for data transmission over standard CAT-5, CAT-5e, and CAT-6 UTP cables.

WINCS02UC Wi-Fi Network Controller Module

The WINCS02IC is a low-power Integrated Circuit (IC) featuring a 2.4 GHz IEEE® 802.11b/g/n-compliant radio with integrated HPA, LNA, RF switches for TX/RX control, and a hardware-based security accelerator, designed to run Microchip's Wi-Fi and Networking stack via Serial Peripheral Interface (SPI).

RNWF02UC Controller ModuleRNWF02UC is a 2.4-GHz IEEE 802.11 b/g/n plug-and-play, Wi-Fi controller module with a U.FL antenna connector and Trust&GO™ secure element. With its on-chip network stack, this module is easy to set up and connect to any cloud platform.  

Back to Top

Troubleshooting

Serial terminal is not showing anything

There are multiple possible reasons why the terminal does not show anything:

  • Verify that the RX-TX signals of the serial cable are properly connected to the RX-TX signals of the board.
  • Verify that the ground signal is properly connected.
  • Verify that the SD card contains the right files.
Terminal shows a WINC Initialize time-out message.
  • Check the connection between the WIxCS02 M.2 Wi-Fi Module and the SAM9x75 Curiosity Board.
  • Make sure the WIxCS02 M.2 Wi-Fi Module is programmed with the correct. M2_Harmony_support.img from the GitHub® repository.
  • Make sure jumper J4 is set to the right position.

When performing the hardware setup (program the WIxCS02 M.2 Wi-Fi Module with the correct firmware image), the terminal shows:

No File Found or Failed to read
the file from sdcard
DFU Failed - looping here

Confirm that the M2_Harmony_support.img from the GitHub repository  has been correctly written to the SD card:

  • Verify that the Harmony_support.bin and boot.bin files are present on the SD card.
Fail to connect the SoftAP or fail to load the webpage
  • Verify that the external antennal is properly connected to the WIxCS02 M.2 Wi-Fi Module.
  • Try to disable the Ethernet connection on the PC.
  • Try to disable the 4G connection on the smartphone.
Terminal shows RomBOOT message
  • Verify that the harmony.bin and boot.bin files are present on the SD card.
  • Verify that the SD card is inserted properly.

Back to Top