SAM9X75 Curiosity Wireless Kit - Wi-Fi® Quick Start Guide for Linux®

Last modified by Microchip on 2026/01/09 08:12

Introduction

Thank you for evaluating the SAM9X75 Curiosity Wireless Kit. This guide will assist you in running the demonstration application designed for the kit. For a more detailed exploration of the kit's features and capabilities, please refer to the links in this guide's "Explore Applications" section.

Pre-Requisites:

  • Confirm the following components are present in the box:
    • SAM9X75 Curiosity Board 
    • LAN8840 EDS2 SODIMM extension board (P/N: EV12N54A)
    • RNBD451 Add-on Board (P/N EV25F14A)
    • WILCS02 M.2 Wi-Fi® Module Card (P/N EV59Y78A)
    • SD card
    • USB Type-A to Micro-USB cable (power)
  • Prepare the following hardware:
    • Linux® PC with an SD card reader and admin rights
    • Serial to USB dongle (FTDI)
  • Install the following applications on the Linux PC
    • A serial terminal software like picocom or minicom
    • balenaEtcher

This quick start guide will help you enable the Soft Access Point (SoftAP) on the SAM9X75 Curiosity Wireless Kit. This allows a smartphone or PC to access a static web page through a browser over Wi-Fi.

Prepare M.2 Module Firmware Update

Program the WIxCS02 M.2 Wi-Fi Module with the correct firmware image.

Download the M2_Linux_support.img file from the GitHub EA03X56A-wifi/m2 

Back to Top


Copy the downloaded file into the SD memory card using balenaEtcher.

Insert the SD memory card into the PC.

Download, install and run balenaEtcher.

Select the downloaded M2_Linux_support.img file.

Select image

Click Select target to download.

Choose target

Select the mounted SD card.

Select target

Select Flash.

Select flash

The SD card will be ready for use once flashing is completed.

Back to Top

Set Up the Board Components

Connect the components as shown in the accompanying images: 

 Insert the flange and antenna assembly into the antenna hole labeled FD1

Secure the antenna into the flange with the antenna wire going under the hole provided. 

Secure antenna ​​Insert antenna through hole

Insert the WIxCS02 M.2 Wi-Fi Module into J20 M.2 connector.
Insert module

Secure the provided screw on the tapped hole provided labeled as STANDOFF1.
Secure screw

Insert the SD card in the SD Boot J14 slot.

Connect the serial USB dongle to the UART DEBUG J35 header.

Set the J24:M.2  I/F SEL to SDIO.

Connect the USB Type-A to Micro-USB cable to the J2 Micro-USB port for power.

Connect components

 

Back to Top

Set Up the SAM9X75 Curiosity Board Serial Terminal

Set up SAM9X75 Curiosity Board Serial Terminal on the PC. 

Identify the serial USB connection by monitoring the last lines of dmesg command (may need sudo rights).

The /dev/ttyUSBx number will be used to configure the terminal emulator.

dmesg output

On the PC, open your favorite terminal emulator with the following settings:

  • Baud Rate: 115200
  • Data: 8-bit
  • Parity: None
  • Stop: 1-bit
  • Flow Control: None

For example with picocom, assuming the serial USB interface is /dev/ttyUSB0:

sudo picocom -b 115200 /dev/ttyUSB0  (sudo rights may be needed)

Back to Top

Verify the M.2 Module Update

Power on the board.

Back to Top


 Confirm using the console that the image copied in Step 2 is used in the Device Firmware Update. 

Confirm console

Back to Top

Prepare the Application Image

Re-use the SD card used in Step 2 to program the Linux application image. 

Back to Top


As already done in Step 2, copy the harmony_application.img in the SD card.

Back to Top


Re-insert the SD card to SD Boot J14 slot. 

Back to Top


Press the RESET (SW3) button on the SAM9X75 Curiosity Board to force a reset. 

When the system is ready, the console terminal you set up earlier in this tutorial will show a prompt.

 Verify the login prompt is shown on the console.

Verify login prompt

Enter "root" to log in. No password is required.

If you do not see the prompt, press the enter key to force the prompt to refresh.

Back to Top

Perform the Test

Perform the test to display the static web page.

In the target console, run the following command:

# /root/Start_AP.sh

The console will display the following selection option:

Display section option

Enter "1" to select Open AP for security AP. 

Wait for the console to display the following logs. This indicates that the softAP mode setup is complete.

Console log display

On the PC, connect to the Wi-Fi access point using the network name "microchip-SoftAP".

Connect to access point

Warning

Ensure there is no active Ethernet connection running simultaneously, as this may prevent the demo page from displaying properly.

On the PC, open a browser, then connect to the access point and enter this address as the URL "http://192.168.1.1".​​​​​​

Enter URL

Confirm the browser displays the following page:

Confirm the browser

Another way to test the SoftAP is to use a smartphone, and connect to the access point using the network name "microchip-SoftAP".

Soft AP smart phone test

Warning

Ensure there is no active internet connection (e.g., 4G, 5G) running simultaneously, as this may prevent the demo page from displaying properly.

On the smartphone, open a browser, then connect to the access point using the address "http://192.168.1.1".

Connect access point

Confirm on the smartphone browser that the following page is displayed:

Confirm page

Back to Top


Congratulations! Your SAM9X75 board running Linux is now connected over Wi-Fi to your PC or smartphone.

What's next? See the following sections for more resources.

Back to Top

Explore Applications

Wireless Applications

Transparent UART communication between a smartphone and the SAM9X75 Curiosity Board using a Bluetooth® LE connection (SAM9X75 Curiosity Wireless Kit - Bluetooth LE Quick Start Guide for Linux)

MPLAB® Harmony Wireless SolutionsRepository containing the MPLAB Harmony v3 Wireless_wifi solutions
MPLAB Harmony Wireless System ServicesRepository containing MPLAB Harmony v3 Wireless system services for RNWF02/WINCS02 device

Ethernet Applications

iPerf networking test between Host PC (as a TCP Client) on Microchip Curiosity Board (as a TCP Server) (SAM9X75 Curiosity LAN Kit - Quick Start Guide for MPLAB Harmony v3)

MPLAB Harmony v3 Solutions

MPLAB Discover Code ExamplesSAM9X75 Peripherals and Drivers code examples
Microchip Graphics SuiteSAM9X75 User's Guide for Microchip Graphics Suite (MGS) for Harmony
Linux solutions

Linux Solutions for SAM9X75

Back to Top

Explore Hardware

SAM9X75 Curiosity LAN KitThe SAM9X75 Curiosity Development Board, featuring the high-performance, ultra-low power SAM9X75D2G MPU with an ARM926EJ-S CPU running up to 800 MHz and integrated 2 Gbit DDR3L memory, serves as the evaluation platform for the SAM9X7 Series MPU devices.

The RNBD451 Add-on Board is a cost-effective development platform for evaluating the RNBD451PE Bluetooth LE module, featuring compliance with the mikroBUS™ standard and an on-board MCP2200 USB-to-UART converter for immediate use without additional hardware.

LAN8840 EDS2 Daughter Card

The EV12N54A LAN8840 EDS2 PHY Daughter Card offers copper Gigabit Ethernet connectivity for Microchip development platforms using the EDS2 interface, featuring the LAN8840 transceiver with PTP support for data transmission over standard CAT-5, CAT-5e, and CAT-6 UTP cables.

WINCS02UC Wi-Fi Network Controller Module

The WINCS02IC is a low-power IC featuring a 2.4 GHz IEEE 802.11b/g/n-compliant radio with integrated HPA, LNA, RF switches for TX/RX control, and a hardware-based security accelerator, designed to run Microchip's Wi-Fi and Networking stack via SPI.

RNWF02UC Controller ModuleRNWF02UC is a 2.4-GHz IEEE® 802.11 b/g/n plug-and-play, Wi-Fi controller module with a U.FL antenna connector and Trust&GO secure element. With its on-chip network stack, this module is easy to set up and connect to any cloud platform.  

Back to Top

Troubleshooting

Common

Serial Terminal is not showing anything.

There are multiple possible reasons why the terminal does not show anything:

  • Double-check that the RX-TX signals of the serial cable are properly connected to the RX-TX signals of the board.
  • Double-check that the ground signal is properly connected.
  • Verify that the SD card contains the right files.

Kernel fails to detect the WIxC02 M.2 module over SDIO.

The log "mmc1: new high speed SDIO card at address 0001" should be printed when the system is booted up if the kernel can detect the WIxCS02 M.2 Wi-Fi module over SDIO. If the Kernel cannot detect the module, the user can make sure:

  • Configure to SDIO at J24 (M.2 I/F SEL) on the SAM9x75 Curiosity Board. 
  • The WIxCS02 M.2 Wi-Fi Module is programmed with WILCS02 Wi-Fi firmware by following the Verify M.2 Module Update steps above.

When programming the WIxCS02 M.2 Wi-Fi module with the correct firmware image, the terminal shows: 

No File Found or Failed to read
the file from sdcard
DFU Failed - looping here

Confirm that the M2_Linux_support.img from the GitHub repository  has been correctly written to the SD card:

  • Verify that the Linux_support.bin and boot.bin files are present on the SD card.
Fail to connect the softAP or fail to load the webpage.
  • Double-check if the external antennal is properly connected to the WIxCS02 M.2 Wi-Fi Module.
  • Try to disable the Ethernet connection on a PC.
  • Try to disable the 4G connection on a smartphone.
Terminal shows RomBoot message.
  • Verify that the SD card contains the right files.
  • Verify that the SD card is inserted properly.

Back to Top