SAM9X75 Curiosity LAN Kit - Quick Start Guide for MPLAB® Harmony v3

Last modified by Microchip on 2026/01/09 08:12

Introduction

Thank you for taking the time to evaluate the SAM9X75 Curiosity LAN Kit. This guide will help you run the demonstration application included with the board. For a deeper dive into the features and capability of the board, refer to the links provided in the "Learn More" section of this guide.

Pre-Requisites:

  • Confirm the following components are present out of the box:
    • SAM9X75 Curiosity Board
    • LAN8840 EDS2 SODIMM extension board (P/N: EV12N54A)
    • SD card
    • USB Type-A to Micro-USB cable (power)
  • Prepare the following hardware:
    • Windows® PC with an SD card reader and administrator rights
    • Serial to USB dongle (FTDI)
    • Ethernet cable
  • Install the following applications on the Windows PC

This quick start guide demonstrates how to perform an iPerf networking test between a Windows PC (acting as the iPerf TCP client) and the SAM9X75 Curiosity Board (acting as the iPerf TCP server).

Two network configurations are possible. Select the preferred one based on your local configuration:

  • Network configuration 1:
    • The board and PC are connected directly with an Ethernet cable. In this case, a static IP will have to be manually assigned to the PC (administrator rights are needed).
  • Network configuration 2:
    • The board and PC are connected through the local network infrastructure or a router. In this case a Dynamic Host Configuration Protocol (DHCP) server will automatically assign an IP address to the board and the PC. (Ensure there are no IT restrictions for plugging the board on the local network.)

See the "Troubleshooting" section at the bottom of this page for more help.

MPLAB® Harmony Demo Setup

Download the iperf.zip from the repository, GitHub_EV31H43A.


Unzip the downloaded iperf.zip file into any directory of your choice. Note the location where the files are unzipped. You will execute the iperf.exe from this location using a command prompt to run the TCP Client.


Download the harmony.img from the repository, GitHub_EV31H43A.


Copy the downloaded file into the SD memory card using balenaEtcher.

Insert the SD memory card into the PC.

Download, install, and run balenaEtcher.

Select the downloaded harmony.img file.

Select Image

Click Select target to download.

Choose Target

Select the mounted SD card.

Select Target

Select Flash.

Flash

The SD card will be ready for use once flashing is completed.


Connect the components as described in the following steps:

Ethernet cable to J5 connector on the LAN8840 EDS2 Daughter Card

The other side of the Ethernet cable needs to be plugged into the PC (network configuration 1) or a wall plug/router (network configuration 2)

SD card inserted on the SD Boot J14 slot

Serial USB dongle to UART DEBUG J35 header on one side and to the PC on the other side

USB Type-A to Micro​​​​-USB cable to J2 Micro​​-USB port for power

Connect components

Back to Top

Set Up the SAM9X75 Curiosity Board Serial Terminal and Start the iPerf TCP Server

Set up SAM9X75 serial terminal on the PC.

On the PC, open a Serial terminal with the following settings:

  • Baud Rate: 115200
  • Data: 8-bit
  • Parity: None
  • Stop: 1-bit
  • Flow Control: None

Open PuTTY.
putty icon

Open Windows Device Manager to find out which COM port to use. Plug and un-plug the Serial-USB dongle and check which COMxx port appears and disappears (COM10 will be used in this example).

Open PuTTY. In the Category pane, expand Connection > Serial and configure the parameters as shown in the accompanying image. (Adapt the COM port to your local setup.)

putty serial

 

In the PuTTY Configuration window,  under Category > Session, choose Serial for Connection type and press Open.

Putty session

Back to Top


Press the RESET (SW3) button on the SAM9X75 Curiosity Board to force a reset.

When the system is ready, the SAM9X75 serial terminal will show a prompt. This is the TCP server running on the Curiosity board and displayed on the PC.

  • In network configuration 1:
    • The board defines its own hardcoded IP address, 192.168.100.11 
  • In network configuration 2:
    • The DHCP server will automatically assign an IP address to the board

Verify that the iPerf MPLAB Harmony application is running and displaying on the SAM9X75 server terminal.
TCP Server terminal

Press the Enter key to show the prompt.
TCP Server terminal

Note the assigned IP address as it will be used to run the iPerf test. 

In this example, corresponding to network configuration 1, the IP address is 192.168.100.11. In case of network configuration 2, the IP address will depend on your local environment.

Back to Top


Start the TCP server on the SAM9X75 Curiosity Board by running the following command:

iperf -s -i 1

The SAM9X75 serial terminal will show that the iPerf application is started and listening: 

TCP Server terminal

Back to Top

Configure the Windows PC and Start the iPerf TCP Client

In network configuration 1:

  • The PC Ethernet IP address and mask must be manually configured (administrator rights are needed).
  • Open Windows network settings (exact steps depend on the Windows version), and switch to manual configuration for the Ethernet interface.
  • Since the board IP is 192.168.100.11, manually configure. For example, the PC to IP is 192.168.100.2 and mask is 255.255.255.0.

IP address setup

In network configuration 2, there is no need to manually set the PC IP address. The DHCP server will automatically assign one.


On the PC, navigate to the folder where iPerf was downloaded in Step 1 and open a Command Prompt.

Command prompt

Back to Top


In the Command Prompt, start the TCP Client iPerf with the following command:

Information

Note that the IP address below used must match the IP address recorded in Step 7.3.

.\iperf.exe -c 192.168.100.11 -p 5001 -i 1 -t 5

This will test the performance of the network transfers between the PC (TCP client) and the SAM9X75 Curiosity Board (TCP server).

The TCP client terminal will show the results of the test: 

TCP Server terminal

Back to Top


Confirm the test results in the SAM9X75 serial terminal:

TCP Server terminal


Congratulations! Your SAM9X75 board running MPLAB Harmony v3 is now connected over Ethernet to your PC.

What's next? See the following sections for more resources.

Back to Top

Troubleshooting

The SAM9X75 serial terminal is not showing anything.

There are multiple possible reasons why the terminal does not show anything:

  • Double-check if the RX-TX signals of the serial cable are properly connected to the RX-TX signals of the board.
  • Double-check that the ground signal is properly connected.
  • Verify if the SD card contains the right files.

Running iperf command on the PC terminal results in a "Connection refused" error.

[1]  tcp connect to 10.14.63.70 port 5001 failed ("Connection refused" error) on 2024-05-31 11:43:21 (US Mountain Standard Time).

Verify that the IP address used when sending the iperf command matches the target IP address.
The terminal shows a RomBOOT message.
  • Verify if the SD card contains the right files.
  • Verify that the SD card is inserted properly.
IT restrictions forbid the plugging in of SD cards in the PC. BalenaEtcher can't be used. 

Another option for programming the SD card is to use the Microchip SAM-BA® In-system Programmer (ISP) tool.

  1. Download and install SAM-BA ISP (v3.9 at least).
  2. Plug the USB Type-A to Micro-USB cable from the PC to J2 Micro-USB port for power and SAM-BA ISP connection.
  3. Plug the SD card in the SAM9X75 board (no more in the PC) and use the following SAM-BA ISP command to program the SD card:

.\sam-ba.exe -p serial -b sam9X75-curiosity -a sdmmc -c write:harmony.img

Back to Top

Learn More

Back to Top