SAM9X75 Curiosity – Writing MPLAB® Harmony v3 Application and at91bootstrap to NOR Flash (QSPI) Memory using SAM-BA® ISP
Introduction
In this training topic, you will write two binary images, harmony.bin (an MPLAB® Harmony v3 Software Framework Application) and boot.bin (Second-stage bootloader, at91bootstrap), to NOR Flash (QSPI) memory on the SAM9X75-Curiosity Development Board using the SAM-BA® In-System Programmer (ISP). Once the images are written, and upon reset, the SAM9X75-Curiosity will boot and run the application.
For this exercise, you will write the binaries that were created in the training topics:
- SAM9X75-EK – Getting Started with MPLAB® Harmony v3 Development: CSP Application: rtt_periodic_timeout
- SAM9X75-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from NOR Flash (QSPI) Memory
Prerequisites
The following are prerequisites to complete this training:
Hardware
For this training, you will use the SAM9X75 Curiosity LAN Kit.
SAM9X75-Curiosity Development Board
Set up the SAM9X75-Curiosity as listed below to the host computer running SAM-BA host application.
Jumpers
- Set the jumpers to their default positions as shown in the "Jumper Summary" section on the "SAM9X75-Curiosity User Guide".
SD Memory Cards
- Ensure no SD memory cards are plugged into the SD card (J14) connector.
Power
- Apply power as shown in the "Power Options" section on the "SAM9X75-Curiosity User Guide".
Console Serial Communications
- To view the target console, connect the host computer running a terminal emulation program per "SAM9X75-Curiosity – Console Serial Communications".
SAM-BA Host to Monitor Serial Communications
- Connect the host computer running the SAM-BA host application to the SAM975-Curiosity per "SAM-BA Host to Monitor Serial Communications".
NOR Flash (QSPI) Memory
The SAM9X75-Curiosity has a 64 Mbit Serial Quad I/O™ (SQI™) Flash memory (U6) (Microchip Technology SST26VF064B) that can be used for booting the system.
The at91bootstrap (boot.bin) binary will be written to locations 0x0 to 0x0003FFFF. The MPLAB Harmony v3 Software Framework application (harmony.bin) binary will be written to locations 0x00040000 to 0x000FFFFF.

Setup SAM-BA Host to Monitor Communications
In this section, you will establish SAM-BA host application communications with the target’s (SAM9X75) SAM-BA monitor. Then you will use the SAM-BA host applet (qspiflash) to erase and then write the boot.bin (at91bootstrap) and harmony.bin (MPLAB Harmony v3 Software Framework application) binary images to NOR Flash (QSPI) memory.
To communicate with the SAM-BA monitor on the target, you must have installed the SAM-BA host on a host computer and connect a Micro-B USB cable to the USB Type-A port (J2) on the SAM9X75-Curiosity.
Ensure there is no SD memory card inserted in slot J14.
Open the NAND BOOT Jumper (J9).
This will disable booting from the NAND memory.
Close the QSPI BOOT Jumper (J10).
This will allow booting from the NOR (QSPI) Flash memory.
Press nRST (Reset) (SW3) push buttons.
The SAM9X75-Curiosity will boot to the SAM-BA monitor and start communications with the SAM-BA host application.
If you have the Console Serial Communications established, you can observe ROMBoot on the Console (terminal emulator) indicating the SAM-BA monitor is running.
Erase NOR Flash (QSPI) Memory
In this section, you will erase the contents of the NOR Flash memory. This is a necessary step before writing data to NOR Flash memory.
Erase the contents of the NOR Flash memory using the following SAM-BA host applet command:
$ sam-ba -p serial -b sam9x75-curiosity -a qspiflash -c erase



Write boot.bin to NOR Flash (QSPI) Memory
In this section, you will write the at91bootstrap binary image, boot.bin, to NOR Flash memory.
Change directory to the location of boot.bin:
<project_directory>\at91bootstrap\build\binaries\boot.bin
Write boot.bin to NOR Flash memory using the following SAM-BA applet command:
$ sam-ba -p serial -b sam9x75-curiosity -a qspiflash -c writeboot:boot.bin -c verifyboot:boot.bin


Write harmony.bin to NOR Flash (QSPI) Memory
In this section, you will write the MPLAB Harmony v3 Software Framework application binary image, harmony.bin, to NOR Flash memory.
Change directory to the location of harmony.bin:
C:\Users\<user>\HarmonyContent\csp_apps_sam_9x7\apps\rtt\rtt_periodic_timeout\firmware\rtt_periodic_timeout_sam_9x75_Curiosity.X\dist\sam_9x75_curiosity\production
Write harmony.bin to NOR Flash memory using the following sam-ba applet command:
$ sam-ba -p serial -b sam9x75-curiosity -a qspiflash -c write:harmony.bin:0x40000 -c verify:harmony.bin:0x40000
The write command is write:<filename>:[<addr>] where <addr> is the Flash Offset for Demo App value in the at91bootstrap configuration (Kconfig). The value 0x200000 you took note of in the training: "SAM9X75-Curiosity – Configure and Build at91bootstrap to Load an MPLAB® Harmony v3 Application from NOR Flash (QSPI) Memory"



Run MPLAB Harmony v3 Application on the Target
Press the nRST (Reset) (SW3) push button to run the application. The RGB LED (LD1) should flash blue. You can also observe the at91bootstrap reading from the NAND Flash memory on the console.

Summary
In this training topic, you wrote the binary files harmony.bin and boot.bin to NOR Flash (QSPI) memory on the SAM9X75-Curiosity and ran the application on the target.