SAMA7D65-Curiosity – Features

Last modified by Microchip on 2026/01/09 08:12

Introduction

This topic describes the features of the SAMA7D65-Curiosity Development Board  with links to additional information. 

Features Summary

The major features of the SAMA7D65-Curiosity are: 

  • SAMA7D65 MPU 
  • Mass Storage 
  • Communications 
  • Debugging 
  • User Interface 
  • Expansion 
  • Power Options 
  • Jumper Summary 

References

Photo of SAMA5D29-Curiosity Development Board

Back to Top

SAMA7D65 MPU

The SAMA7D65 is a high-performance Arm® Cortex®-A7 CPU embedded microprocessor (MPU) running up to 1 GHz. 

SAMA5D29-Curiosity - Processor

Back to Top

Mass Storage

There are three mass storage options available on the development board: 64 Mb Serial Quad I/O™ (SQI™) Flash with EUI-48 and EUI-64 (U9), NAND Flash Memory (U8), and Secure Digital Multimedia Card (SDMMC) (J10).

SAMA5D29-Curiosity - Mass Storage

64 Mb Serial Quad I/O™ (SQI™) Flash with EUI-48 and EUI-64 (U9)

U9 is a 64 Mb Serial Quad I/O (SQI) Flash with EUI-48 and EUI-64 memory (Microchip SST26VF064BEUI). It is connected to the Quad SPI Interface 0 (QSPI0) peripheral of the SAMA7D65. 

NAND Flash Memory (U8)

U8 is a 4-Gbit SLC NAND Flash memory Macronix MX30LF4G28AD-XKI.

Secure Digital Multimedia Card (SDMMC) (J10)

J10 is a Secure Digital (SD) or MultiMediaCard (MMC) memory card slot. It is connected to the Secure Digital MultiMediaCard port 1 (SDMMC1) peripheral of the SAMA7D65. 

SAMA5D29-Curiosity - Mass Storage

J10 can accommodate SD format radio modules. See the SAMA7D65-Curiosity User’s Guide for more information. 

Back to Top

Communications

The SAMA7D65-Curiosity provides wired communications via Ethernet, USB, CAN, and wireless communications from M2 wireless interface.

SAMA5D29-Curiosity - Communications

Ethernet (J15)

The SAMA7D65-Curiosity contains a 10/100/1000 Reduced Gigabit Media-Independent Ethernet (RGMII) and Serial Peripheral Interface (SPI) SODIMM interface available on connector J15. Microchip provides a wide range of compatible Ethernet daughter boards that can be used for testing and evaluation. See the SAMA7D65-Curiosity User’s Guide for more information. 

USB (J3, J23 and J24)

The SAMA7D65-Curiosity features three USB communication ports named USB-A (J3), USB-B (J23) and USB-C (J24). 

The USB-A port (J3) acts only as a USB device interface and is accessed via USB Type-C connector J3. 

The USB-A port (J3) can be used as a source of power for the development board. In most cases, this port is limited to 500 mA. See Power Options below. 

The USB-A port (J3) is used as the default serial port used to communicate with the SAM-BA® Monitor resident in the MPU. 

The USB-B port (J23) and USB-C port (J24) acts as a host and is accessed via USB Type-A connectors J23 and J24. 

Controller Area Network (CAN) Flexible Data-Rate (FD)

The SAMA7D65 MPU contains three dedicated CAN-FD interfaces, each equipped with an MCP2542FD CAN transceiver.

Each CAN port features a 3-pin terminal block named CAN1 (J29), CAN2 (J30) and CAN3 (J31). Wires can be plugged in the terminal blocks without the use of a screwdriver.

Wireless M.2 interface (J11)

The SAMA7D65-Curiosity board embeds an M.2 connector to interconnect with Wireless add-on cards. Only wireless cards cards compatible with the PCIe M.2 Key E slot (J11) are supported. 

M.2 (formerly known as NGFF) is a small form factor card and connector that supports applications such as Wi-Fi®, WLAN, USB, PCI Express® (PCIe®) and SATA, as defined in the PCI-SIG® M.2 Specification.

The M.2 slot also features a Universal Asynchronous Receiver Transmitter (UART) interface with hardware flow control for the Bluetooth® component
of the add-on card.

The main interface integrated in the M.2 slot is SDMMC2, for the Wi-Fi component of the add-on
card. An optional SPI interface is also multiplexed with the SDMMC2 pins and is available by
changing the JP5 jumper position on the J12 header.

Back to Top

Debugging

There is one method of debugging the SAMA7D65-Curiosity via JTAG (J38) using MPLAB® PIC™kit 5. In addition, a dedicated serial port for debugging and Console Serial Communications (J35). 

SAMA5D29-Curiosity - Debugging

JTAG (J38)

A JTAG interface to the SAMA7D65-Curiosity is provided by 20-pin connector J38. This facilitates software development and debugging by connecting an external JTAG debugger such as MPLAB PICkit 5

The JTAG interface signals voltage levels are 3.3V. 

Serial Debug Port (J35)

The Serial Debug Port (J35) is a dedicated TTL-level serial port connection between the SAMA7D65 and J35. A level shifter (U19) allows either 3.3 or 5.0 VDC levels. To interface between J35 and the host computer, you will need a USB-to-Serial (3.3 or 5.0 VDC) TTL level adapter with a 6-pin single-in-line 0.1” pitch connector.  

Take care to align Pin 1 (GND) of the header J35 to the USB-to-Serial adapter Pin 1 (look for an arrow on the connector and a black wire). 

A terminal emulation program running on a host computer provides a user interface to interact with the target console. 

For more information, see the SAMA7D65-Curiosity: Console Serial Communications page.

Back to Top

User Interface

SAMA5D29-Curiosity - User Interface

Red-Green-Blue (RGB) LED (D11)

The SAMA7D65-Curiosity features one RGB LED (D11). 

Pushbuttons (SW1-SW4)

The SAMA7D65-Curiosity contains three pushbuttons: 

  • WKUP (SW1): When pressed the MPU wakes up from a low-power state.
  • USER (SW2): User push button is the connector to PIO PA17 and is available for the user’s usage. 
  • RESET (SW4): Reset push button; when pressed the system resets. 
  • START (SW3): When pressed it will initiate the PMIC start-up sequence if the buck converters are off. The PMIC will also assert the SAMA7D65 wakeup (WKUP) signal to wake the MPU from a low-power state. 

LVDS Interface (J17)

The SAMA7D65-Curiosity contains a 30-pin FPC LVDS display connector. An external LVDS display can be connected to the J17 30-pin FPC connector.

MIPI® DSI Display Interface (J16)

The SAMA7D65-Curiosity contains a 34-pin FPC MIPI® display connector. An external MIPI display can be connected to the J16 34-pin FPC connector.

Back to Top

Expansion

SAMA5D29-Curiosity - Expansion

mikroBUS™ (J25 and J26)

mikroBUS™ socket is a proprietary communication and plugin standard for small interface boards called Click boards™ that extends the capabilities of the development board by offering SPI, UART, TWI, and PWM-based sensors and devices. They are made by MikroElektronika, a producer and retailer of hardware and software tools for developing embedded systems. 

GPIO/Raspberry Pi® Connector(J18)

The SAMA7D65-Curiosity contains a 40-pin GPIO connector (J18) for use. This connector is compatible with the Raspberry Pi® expansion header. 

Tamper (J33) and System Signals (J34) Connectors (Not populated)

The SAMA7D65-Curiosity board provides two tamper pins for static or dynamic intrusion detection on connector J33 (not populated).  

The PMIC High-Power Mode (HPM) signal, used to enable the PMIC High-Power mode, is present on J34 pin 4. 

Unused I/O signals from the SAMA7D65 are routed to connectors J33 and J34 (not populated). 

Signal NameDescription
JTAGSEL (J33)JTAG boundary scan mode enable 
SHDN (J33)Enable/disable external power supply circuit 
AUDIOCLK (J33)Dedicated audio clock signal
MCP16502_HPM (J34)PMIC High Power mode enable
NRST_OUT (J34)Peripheral reset output
NRST (J34)Processor reset input
SEL_VLDO1 (J34)Selects the output voltage of LDO1 of the MCP16502 PMIC

Back to Top

Power Options

There are two options to power the SAMA7D65-Curiosity: USB-A Port (J3) and DC Jack (J1).

SAMA5D29-Curiosity - Power Options

USB-A Port (J3)

The USB-A port (J3) is a USB-C connector and can be used as a power source for the development board. In most cases, this port is limited to 500 mA. 

DC Jack (J1)

The SAMA7D65-Curisosity can be powered by an external 5.0 VDC power supply. The connector (J1) is a 2.1 mm coaxial center-positive. 

DO NOT exceed 6.0 VDC on DC Jack (J1). 

If both J1 and J3 are powered at the same time, automatic switching circuitry prioritizes power from the DC Jack (J1).  

Back to Top

Jumper Summary

The SAMA7D65-Curiosity jumpers are as follows: 

SAMA5D29-Curiosity - Jumpers

Jumper J4 – VDDBU Current Measurement:

  • Closed: (default) 
  • Open: Removing the jumper will remove power to VDDBU and reset the Boot Sequence
    Controller Configuration register (BSC_CR) to their initial configuration. 

Ensure the SAMA7D65-Curiosity Development Board is powered off before removing jumper J4. 

Jumper J4 must be in place for the proper operation of the MPU.  

Jumper J39 – Serial Quad I/O (SQI) Flash Boot:

  • Closed: Enable boot (default) 
  • Open: Disable boot 

Jumper J36 – NAND Flash Boot:

  • Closed: Enable boot (default) 
  • Open: Disable 

Jumper J32 – CAN1, CAN2 and CAN3 Transceiver:

  • Closed: Enable boot (default) 
  • Open: Disable 

Jumper J2 – Extra 3.3V and 2.5V source select

  • 1-2 Closed: Enable extra power source from VDD_3V3
  • 2-3 Closed: Enable extra power source from 5V_MAIN
  • Open: Disable 

Jumper J6 – PAC1934 TWCK selection on USB

  • 1-2 Closed: Enable TWCK selection on USB (default) 
  • 2-3 Closed: Enable TWCK selection on MPU
  • Open: Disable 

Jumper J7 – PAC1934 TWD selection on USB

  • 1-2 Closed: Enable TWD selection on USB (default) 
  • 2-3 Closed: Enable TWD selection on MPU 
  • Open: Disable 

Jumper J12 – M.2 SDIO/SPI interface selection

  • 1-2 Closed: Enable SDIO (default) 
  • 2-3 Closed: Enable SPI
  • Open: Disable 

Back to Top