Memory Xplorer Write, Read, and Erase Operations
How to Perform Write, Read, and Erase Operations in Memory Xplorer
Write Operation
Select the Write button at the top of the Array Tools panel to open the Write Panel. Refer to Array Tools Panel section for details.
Select whether you want to write the array in Page or Byte mode. Page writes require less time than Byte writes. Page size varies by device, refer to the device product datasheet for details.

Make your desired changes to the Hex Editor memory viewer. See the Hex Editor section for more information.
When changes have been made to a memory array and sufficient information has been provided to complete the operation, the Write button will turn green. This indicates a write is needed to synchronize the Hex Editor data with device memory contents. Refer to Array Tools Panel section for available options.
Click the green Start button to start the write operation.

The memory view in the Hex Editor will indicate progress status . Once programming is complete, highlights are removed.

Read Operation
Select the Read selector button at the top of the Array Tools panel to open the Read Panel. Refer to the Array Tools Panel section for details.

Select a range of memory to read (see Selecting Memory Addresses section for details). Once a memory range has been selected, the Read button will turn green.
Click the Read button to start the operation.

The memory view in the Hex Editor will indicate progress status . Once the read operation is complete, highlights are removed.

Erase Operation
Select the Erase selector button at the top of the Array Tools panel to open the Erase Panel. Refer to the Array Tools Panel section for details.

Select an Erase Mode; Device, Sector or Page. Device will erase all memory regions and return them to their factory default values. For Sector or Page, select a range of memory to be erased (see Selecting Memory Addresses section for details). If a partial sector or page is included, the entire portion will be included in the erase operation (see Erase Button section for more information). Once a memory range has been selected, the Erase Selection button will turn green.
Click the Read button to start the operation.

The memory view in the Hex Editor will indicate progress status . Once the read operation is complete, highlights are removed.

Learn more
- Memory Xplorer Embedded Memory Evaluation Platform
- Evaluation kits
- SPI Introduction
- I2C Bus Introduction
- What is Single Wire Interface (SWI) protocol?
- Unique ID UID)
- Media Access Control (MAC) addresses
- EEPROM Endurance Tutorial (AN1019)
- Sample order page
- Serial EEPROM page
- Microchip Purchasing and Client Services
- Intel formatted hex files