Hardware Guide for SAM9x75 Curiosity with Raspberry Pi® 800x480 7-inch MIPI LCD
                  Last modified by Microchip on 2024/09/03 14:44
              
      Required Hardware (HW)
| Product Number | Description | 
|---|---|
| EV31H43A | SAM9x75 Curiosity Development Board | 
| SKU 22293 | Raspberry Pi® 800 x 480 7 inch MIPI DSI LCD | 
| B09BB37D42 | Waveshare DSI FFC Flexible Flat Cable 15cm | 
| Micro-USB cable or 5V power adapter for SAM9x75 Curiosity power supply | |
| Micro-USB cable for display power supply | |
| microSD card for firmware binaries | 
HW Setup
Refer to the accompanying images for instructions on how to connect the display to the 9x75 Curiosity board.
The cable that comes with the display will not work with the Curiosity board. Use the Waveshare DSI FFC Flexible Flat Cable to connect the display to the board as shown in Figure 1. The Curiosity board and the display are separately powered via USB.
The microSD card with the firmware binaries goes to the microSD card slot labeled SD BOOT.

Figure 1
Figures 2 and 3 show close-ups of how the cable is connected to the Curiosity board and display.

Figure 2

Figure 3
Figure 4 shows the display and board side-by-side:

Figure 4