Hardware Guide for SAM9x75 Curiosity with 5" LVDS WVGA maXTouch® Technology Display Module
Last modified by Microchip on 2024/09/03 14:45
Required Hardware (HW)
| Product Number | Description |
|---|---|
| EV31H43A | SAM9x75 Curiosity Development Board |
| AC69T88A | 5" LVDS WVGA 800 x 480 maXTouch® Technology Display module |
| Micro USB or 5V power adapter for SAM9x75 Curiosity power supply | |
| microSD card for firmware binaries |
HW Setup
Refer to the included images for instructions on how to connect the display to the 9x75 Curiosity board.
The display comes with an LVDS cable that is used to connect the display to the board as shown in Figure 1. The display is powered from the Curiosity board.
The microSD card with the firmware binaries goes to the microSD card slot labeled SD BOOT.

Figure 1
Here's a close-up of how the display connects to the Curiosity board using the LVDS interface.

Figure 2
The display can be mounted to the board using the 8-pin headers.

Figure 3
When mounted, the hardware setup should appear as shown in Figure 4.

Figure 4