Line Widget Documentation
Introduction
A Line Widget is a graphical user interface component used to draw straight lines on the screen.
It's a straightforward and effective way to add visual elements such as dividers, borders, or indicators to the interface. The start and end points of the line can be precisely defined using coordinates, allowing for flexible placement within the Graphical User Interface (GUI). This widget is non-interactive and serves purely as a visual aid to enhance the layout and organization of the interface.
This page covers the following topics:
- Creating and customizing Line Widgets using Microchip Graphics Suite (MGS) Harmony Composer
- Line Widget properties
- Handling Line Widget properties and events through application code
- Line Widget example project
- Application Program Interfaces (APIs) specific to Line Widgets
Designing Line Widget Using MGS Harmony Composer
Follow these steps to add a Line Widget to your design:
Select and drag the LineWidget to your screen designer workspace as shown in Figure 1.
Figure 1: Adding LineWidget to screen
To customize the LineWidget, select the widget from the Screen Tree and modify its properties using the Object Editor.
Figure 2: Object Editor
Managing Line Widget Schemes
Schemes control the look and feel of a widget.
To learn how to set the scheme for an image, click on the question mark
button next to the Scheme property editor of the Object Editor.
Figure 3: Button to launch Scheme helper window
This will launch the Line Scheme Helper window containing tips on how different sections of the scheme settings manipulate various elements of the line.

Figure 4: Line Scheme Helper
The following is an example color scheme and the resulting appearance of the LineWidget:
Figure 5: Choosing Scheme for LineWidget
The information provided by the Line Widget Scheme Helper and the example color scheme is summarized in Figure 6.

Figure 6: LineWidget color scheme
Line Widget Properties
You can set the following properties of the Line Widget using the Object Editor:
Name This will be used to reference the LineWidget by the application. Example-
Screen0_LineWidget_0
Line (P1X, P1Y) and (P2X, P2Y) specify the start and end positions in pixels of the line within the widget.
Managing Line Widget Through Programming
Once the graphical design is completed using MGS Harmony Composer, MCC generates the required code for all the widgets based on the properties set in the Object Editor. To learn more about the process flow between designing a UI and developing application code, refer to the "Designing an Application with Microchip Graphics Suite (MGS)" page.
Let us suppose that a new line widget is created with the following properties in MGS Harmony Composer:
Figure 7: LineWidget properties
For the Line Widget with the properties shown in Figure 7, MCC will automatically generate the following lines of code in src\confg\default\gfx\legato\generated\screen\le_gen_screen_Screen0.c:
- A new Line Widget is created by the variable name Screen0_LineWidget_0
Screen0_LineWidget_0 = leLineWidget_New();
- Its position is set to pixel location 186x67.
Screen0_LineWidget_0->fn->setPosition(Screen0_LineWidget_0, 186, 67);
- The Line Widget size is set to have a width of 100 and a height of 98.
Screen0_LineWidget_0->fn->setSize(Screen0_LineWidget_0, 100, 98);
- The required scheme for the Line Widget is selected.
Screen0_LineWidget_0->fn->setScheme(Screen0_LineWidget_0, &LineScheme);
- The start point position of the Line within the Widget is set.
Screen0_LineWidget_0->fn->setStartPoint(Screen0_LineWidget_0, 0, 50);
- The endpoint position of the Line within the Widget is also selected.
Screen0_LineWidget_0->fn->setEndPoint(Screen0_LineWidget_0, 100, 50);
- Finally, the Line Widget is added to the screen.
root0->fn->addChild(root0, (leWidget*)Screen0_LineWidget_0);
Line Widget Example Project
Refer to the Line Widget Example Project in GitHub
In this example, we show:
- How to create a Line Widget,
- How to change the color of a line on a button press, by selecting a different color scheme
- How to rotate the line, by changing the line start and end position
MGS Harmony Web Simulator Output
The callback function for handling the button release event is defined in the app.c file.
{
// Get the current start and end points of the line
int32_t startX = Screen0_LineWidget_0->x1;
int32_t startY = Screen0_LineWidget_0->y1;
int32_t endX = Screen0_LineWidget_0->x2;
int32_t endY = Screen0_LineWidget_0->y2;
// Calculate the center of the line
int32_t centerX = (startX + endX) / 2;
int32_t centerY = (startY + endY) / 2;
// Translate points to origin (center of the line)
int32_t translatedStartX = startX - centerX;
int32_t translatedStartY = startY - centerY;
int32_t translatedEndX = endX - centerX;
int32_t translatedEndY = endY - centerY;
// Rotate points by 90 degrees
int32_t rotatedStartX = -translatedStartY;
int32_t rotatedStartY = translatedStartX;
int32_t rotatedEndX = -translatedEndY;
int32_t rotatedEndY = translatedEndX;
// Translate points back to original position
int32_t newStartX = rotatedStartX + centerX;
int32_t newStartY = rotatedStartY + centerY;
int32_t newEndX = rotatedEndX + centerX;
int32_t newEndY = rotatedEndY + centerY;
// Set the new start and end points
Screen0_LineWidget_0->fn->setStartPoint(Screen0_LineWidget_0, newStartX, newStartY);
Screen0_LineWidget_0->fn->setEndPoint(Screen0_LineWidget_0, newEndX, newEndY);
if ((Screen0_LineWidget_0->fn->getScheme(Screen0_LineWidget_0) == &LineScheme))
{
Screen0_LineWidget_0->fn->setScheme(Screen0_LineWidget_0, &RedScheme);
}
else
{
Screen0_LineWidget_0->fn->setScheme(Screen0_LineWidget_0, &LineScheme);
}
}
Line Widget APIs Description
This section describes the APIs specific to the Line Widget. For a description of APIs common to all widgets, refer to the "Widget APIs Description" section.
getStartPoint()
leResult getStartPoint(const leLineWidget* _this, lePoint* pnt)
- Gets the start point (x1,y1) of the line
- Returns LE_SUCCESS or LE_FAILURE
Parameters
| leLineWidget* | _this | Line widget pointer to operate on |
| lePoint* | pnt | pnt is a pointer to a lePoint structure, which is expected to hold the coordinates (x, y) of a specific point. |
setStartPoint()
leResult setStartPoint(leLineWidget* _this, int32_t x,
int32_t y)
- Sets the start point (x1,y1) of the line
- Returns LE_SUCCESS or LE_FAILURE
Parameters
| leLineWidget* | _this | Line Widget pointer to operate on |
| int32_t | x | Variable to hold x coordinate of start point |
| int32_t | y | Variable to hold y coordinate of start point |
getEndPoint()
leResult getEndPoint(const leLineWidget* _this, lePoint* pnt)
- Gets the endpoint (x2,y2) of the line
- Returns LE_SUCCESS or LE_FAILURE
Parameters
| leLineWidget* | _this | Line widget pointer to operate on |
| lePoint* | pnt | pnt is a pointer to a lePoint structure, which is expected to hold the coordinates (x, y) of a specific point. |
setEndPoint()
leResult setEndPoint(leLineWidget* _this, int32_t x,
int32_t y)
- Sets the endpoint (x2,y2) of the line
- Returns LE_SUCCESS or LE_FAILURE
Parameters
| leLineWidget* | _this | Line widget pointer to operate on |
| int32_t | x | Variable to hold x coordinate of start point |
| int32_t | y | Variable to hold y coordinate of start point |