Using Bitmap Images
Using Bitmap Images in a Graphics Application
Graphic Images
Bitmap Images
- Bitmap images are binary files that contain a pixel-by-pixel description of a graphical image. The value of each pixel is stored in one or more bits of data as defined by the color depth, or Bits Per Pixel (BPP).
Importing Bitmap Images
Step-by-Step Instructions:
Importing Images to an MLA Graphics Project
The Graphics Resource Converter (GRC) utility is used to import graphics images. (This is the same utility used to import fonts). The GRC can import images from bitmap files (BMP) or JPEG files (JPG or JPEG).
The GRC is located in the MLA Installation directory, …microchip/mla/vYYYY_MM_DD/framework/gfx/utilities/grc.
Linux® and macOS® users launch the resource converter by executing grc.jar, and Microsoft® Windows® users invoke it by executing launch_grc.bat.
Using Bitmap Images
Once the image has been imported into the project and rebuilt, you will be able to display the image on the screen. To reference an imported image, you refer to the image by the name given in the header file. When an image file is converted, you will be prompted to enter the name of the file to store the image. This example uses NewImage as the name of the image file.


Example of MPLAB® X IDE project tree with the assembly (.s), header (.h), and C (.c) files added.
Function Used to Output an Image
GFX_ImageDraw(left, top, &image): Displays the image on the screen at the coordinates designated.


Helpful Functions to Position Images on the Screen
The following functions can be useful to position your images (and objects) on the screen:
GFX_MaxXGet(): Returns the width (in pixels) of the display
GFX_MaxYGet(): Returns the height (in pixels) of the display
GFX_ImageWidthGet(GFX_RESOURCE_HDR pImage): Returns the width of the image in pixels.
GFX_ImageHeightGet(GFX_RESOURCE_HDR pImage): Returns the height of the image in pixels.


To get a complete list of the functions available for working with bitmap images open
help_mlagfx.jar located in ..microchip/mla/vYYYY_MM_DD/doc…