Timing Touch Events in Graphics Applications
Summary
In some applications, it is necessary to time how long an object is touched. Timing touch events allows the application to change a system value based on the length of time an object on the display is touched.
One example of a continuous touch event could be a dimmer switch for lighting. In addition to changing the lighting value each time an up or down button is pressed, the system may be configured to gradually increase or decrease the lighting in response to the user keeping their finger on either the up or down button.
This article describes the process and steps needed to take action based on the amount of time an object has been touched.
Overview
Processing Timed Events
The process for determining time intervals takes several steps:
- When an event is first detected the Message Callback function sets a flag indicating a touch event that needs to be timed is taking place. The message callback function will then read the current system time from the tick module, add a calculated delay period, and store this value.
- On each iteration of the main loop the Draw Callback function tests the flag to see if a continuous touch event is taking place. If a continuous touch event is active, the current system time is tested to see if the desired time delay has passed. When the desired time interval has passed, the Draw Callback function takes the appropriate system action, then calculates the next delay time interval.
- When the Message Callback function detects the touch event has been RELEASED the flag telling the Draw Callback to monitor the timed touch event is cleared.
To implement continuous touch timing, three elements of the Graphics library must be used in conjunction with each other:
- Message Callback function (GFX_GOL_ObjectMessageCallback)
- Draw Callback function (GFX_GOL_ObjectDrawCallback)
- The Tick Module
Message Callback Function
The Message Callback function is called by GFX_GOL_ObjectMessage each time a touch event has been detected. To monitor the length of time a touch event occurs the Message Callback Function first records that a "timed" touch event is occurring by setting a global variable when the touch is detected. The Message Callback then determines what time to take the incremental system action.

Draw Callback Function
The Draw Callback Function, described in detail below, is called by GFX_GOL_ObjectListDraw each time through the main loop. The draw callback function checks to see if the Message Callback function has set the flag indicating a particular touch event is happening. If a timed touch event is taking place and the desired time interval has passed the Draw Callback function takes the desired incremental action.

Tick Module (System Timing Module)
The tick module is a system resource that keeps track of the system time. Typically the tick module uses a timer interrupt to increment a variable at a constant interval. A description of how to set up and use the tick module is covered later on this page.
Using the Draw Callback Function
The draw callback function is implemented by the application developer. The developer first writes a function to perform the Draw Callback tasks. This function may be given any valid function name. The function GFX_GOL_DrawCallbackSet is then used to assign the user-written function and the Draw Callback function. Each time GFX_GOL_ObjectListDraw is executed the user written draw callback function will be called.

Setting up the Tick Module
Tick Module Location in an MLA Application
The functions needed to start up and implement the tick module in MLA applications are located in the system.c file. In Microchip-supplied graphics projects, system.c can be accessed in the project tree under the system_config directory. There is a sub-directory under system_config for every project configuration. Each of the sub-directories contains a system.c file, which is written to implement the tick function for the specific MCU used in the corresponding project configuration. The file properties of the multiple system.c files are set so that only the version of system.c for the current configuration is included in the build.

Key Functionality Included in the MLA Tick Module
The tick module includes:
- A tick module initialization routine that needs to be called for the tick module to operate.
- A timer-specific Interrupt Service Routine (ISR) that increments a data variable at specific intervals.
- Various #define functions and variable declarations to provide the application programmer with an easy method of calculating delay intervals.
- The ability to read the current value of the system tick variable.
Example Code: Timing a Touch Event
A button called UPbutton has been created and placed on the display list. In addition to the display, the MCU is connected to a motor. The speed of this motor is increased each time the UPMotor function is called.
In this example, the tick module uses a timer interrupt and places the system time in a uint32 variable called tick.
Steps to Implement this Example
Calculate and Define Delay Interval
The essential calculation is to determine how much the tick timer will increment in a given time interval. This calculation requires knowledge of the system clock frequency and both the period register and pre-scale value for the timer used by the tick module.

To implement this calculation the following #define functions are added to the project:


Modify the Message Callback Function
When Msg informs the message callback function that the button has been PRESSED:
- The state variable touch_state is set to touched
- DoneAt is loaded with a value that the tick timer will contain in half-second units
When the Msg indicates the button has been RELEASED:
- touch_state is set to not_touched

Create the Draw Callback Function
When both (touch_state == pressed) and the time interval has passed:
- UPmotor() is called
- DoneAT is loaded with the value for tick in the next half second.

Set the Draw Callback Function