SAM-BA® In-System Programmer Target Console Serial Communications
Introduction
The Target Console (also known as DEBUG, Device Console, Applet Console, or simply Console) is a serial communications port (generally a Universal Asynchronous Receiver Transmitter (UART)) on the target device that can communicate with a terminal emulation program on a host computer. It provides status information from operating systems, such as Linux®, and debug information from utility programs (see the "SAM-BA® In-System Programmer - Applets" page).

As shown in the SAMA5D2 Series MPU block diagram, the UART is configured as the Target Console by the Boot Configuration Word. A serial-to-USB converter is generally needed for the USB port on a host computer to communicate with a two-wire UART of the target. On some evaluation kits, the serial-to-USB converter is on-board. This Target Console is also called the DEBUG port.
When the host computer is connected to the evaluation kit or separate serial-to-USB converter, the host computer will enumerate as a Communication Device Class (CDC). Take note of the USB port designation as it will be needed to configure the Terminal Emulation Program.
Terminal Emulation Program
Download, install, and configure a Terminal Emulation program onto your host computer.
Serial Communications Port
Connect the host computer running the terminal emulation program to the target console serial communications port. The host computer will enumerate as a CDC. Take note of the USB port designation as it will be needed to configure the Terminal Emulation Program
Evaluation Kit
If you are using an evaluation kit, the user manual will identify the port used for the console. The -b, --board option will configure the SAM-BA host to communicate with the default console of the evaluation kit.
Custom Board
If you are developing with a custom board design, the Target Console can be configured by the Boot Configuration of the target device. In addition, the console can be set using the -d, --device <console_instance>:<console_ioset> option.
Syntax: sama5d2:[<instance>]:[<ioset>]
Parameters:
instance - Serial console peripheral number
ioset - Serial console I/O set
Examples:
sama5d2 - use default device/board settings
sama5d2:1:2 - use fully custom settings (peripheral number 1, I/O set 2)
sama5d2::2 - use default device/board settings but force use of I/O set 2
Note:
Peripheral numbers and I/O sets are device specific. Please see device documentation in 'doc' directory
Applet Trace Level
Applet trace level verbosity can be controlled with the -t, --tracelevel option. See the "SAM-BA In-System Programmer - Applets" page for more information.