AC162062, AC162079, AC162087, AC162091

Last modified by Microchip on 2023/12/20 19:20

Header Identification

The AC number is used for ordering the Processor Extension Pak, which contains the debug header. However, this number is not on the header, as the board may be used for multiple headers by inserting different -ICE/-ICD devices. To identify these headers, use the following information.

AC Number-ICE/-ICD DeviceBoard Assembly Number
AC162062PIC18F87J10-ICE02-01830
AC162079PIC18F85J90-ICE
AC162087PIC18F87J50-ICE
AC162091PIC18F87J11-ICE

Header Setup and Operation - AC162062

For this header, there are no jumpers/switches. MPLAB® X IDE will use its selected device to choose the correct device to emulate.

Test points are available on this header to check the following: Vdd, Vddcore and ground.

Warning

Caution

Header Damage.
This header cannot be plugged directly into the
PICDEM™ HPC Explorer Board! Device damage will result.
BoardZap.jpg

The PICDEM HPC Explorer Board is 5V, whereas the ICD device on the header is 3.6V max. Therefore, modification to the demo board is necessary before the header can be used.

  1. Switch S3 should be set to ICE.
  2. Jumper J2 must be connected as shown in the figure to modify the operating voltage. See the demo board documentation for more information.
Figure: Demo Board J2 Connections

Figure: Demo Board J2 Connections

Back to top

Header Setup and Operation – AC162079, AC162087, AC162091

For these headers, there are no jumpers/switches. MPLAB® X IDE will use its selected device to choose the correct device to emulate.

Test points are available on this header to check the following: Vdd, Vddcore and ground.

Back to top

Header Limitations

Sometimes a header device (-ICE/-ICD) has operational issues or errata. To determine if a device on a header has limitations, see your hardware tool documentation.

Back to top

Header Dimensions

The accompanying image lists the dimensions for the debug header. Dimensions are design values in inches.

If the length and/or width of the debug header is too large a footprint for the target board, consider using stand-offs, transition sockets or other extenders in the header connection socket to raise the header above the target.

Figure: Dimensions - AC162062, AC162079, AC162087, AC162091

Figure: Dimensions - AC162062, AC162079, AC162087, AC162091
​

Back to top