Atmel-ICE Configuration Options
Set up Atmel-ICE debugger options on the property pages of the Project Properties dialog.
Open the Project Properties dialog by doing one of the following:
Click the project name in the Projects window and select File > Project Properties.
Right-click the project name in the Projects window and select Properties.
Under Categories, click on Atmel-ICE Tool.
Select Property Pages from Options Categories. Click on an option to see its description in the text box below it. Click to the right of an option to change it.
Available Category Options
Memories to Program
Select the memories to be programmed into the target.
If Erase All Before Program is selected under Program Options, then all device memory will be erased before programming. To select only certain memories to program after erase, check the specific memory type. To preserve the value of memory of different types, check to preserve that memory type and check the specific memory type. Checking Preserve Memory writes the current contents to a buffer before erase. Checking Memory writes the contents back into that memory after erase, where Memory is the type of memory, such as EEPROM.
Table: Memories to Program, Option Category
| Auto select memories and ranges | Allow the tool to select memories: The debugger uses your selected device and default settings to determine what to program. Manually select memories and ranges: You select the type and range of memory to program (see below). |
| Memory | Check to program Memory, where Memory is the type of memory. Types available are dependent on the project device and can include Data Flash, EEPROM, etc. Care should be taken when programming configuration bits, as invalid values, may cause unintended results. |
| Program Memory | Check to program the target program memory range specified below. |
| Program Memory Range(s) (hex)1 | The starting and ending hex address range in program memory for programming, reading, or verification. Note: the address range does not apply to the Erase function. The Erase function will erase all data on the device. |
| Preserve Program Memory | Check to not program the target program memory range specified below. Ensure code is NOT code protected. |
| Preserve Program Memory Range(s) (hex)2 | The starting and ending hex address range in target program memory to preserve when programming, reading, or verifying. This memory is read from the target and overlayed with existing MPLAB® X IDE memory. |
| Preserve Memory | Check to not program the target memory range specified below. Ensure code is NOT code protected. |
| Preserve Memory Range(s) (hex)2 | The starting and ending hex address range in target memory to preserve when programming, reading, or verifying. This memory is read from the target and overlayed with existing MPLAB X IDE memory. |
Program Options
Choose whether or not to erase all memory before programming.
Table: Program Options, Option Category
| Erase All Before Program | Check to erase all memory before programming begins. Unless programming new or already erased devices, it is important to have this box checked. If it is not checked, the device is not erased and the program code will be merged with the code already in the device. |
Debug Options
Choose the options for debugging with Atmel-ICE.
Table: Debug Options, Option Category
| Use software breakpoints | Check to use software breakpoints instead of any hardware breakpoints. |
Firmware
Select debug tool firmware updates.
Table: Firmware Option Category
| Firmware Update Options | Use the latest firmware: Let MPLAB X IDE automatically download the correct firmware. Select firmware file: Use the Firmware File specified below. Do not change firmware: Do not automatically download updated firmware. |
| Firmware File | Click in the right-hand text box to search for a firmware file to associate with the debug tool. |
Related Topic: Emulator Firmware Upgrade
Communication
Choose the communication interface between the Atmel-ICE debugger and target.
Table: Communication Option Category
| Interface | Select the device-supported Atmel-ICE interface: JTAG, SWD, ISP, debugWIRE, UPDI, or TPI. For more information, see the "Features" section on "Atmel-ICE Debugger Overview". |
| Speed (MHz) | Enter a speed of operation based on the interface chosen. |