Atmel START: Introduction Videos with SAM L21 Project Development and Debug
Last modified by Microchip on 2024/06/10 11:14
Contents
- Introduction to the video series
- Hello World!
- Best Practice Code Cleanup
- Configuring and Reading the ADC
- ADC with Delay, Visualization
- ADC with Timer Callback, Visualization
- ADC Timer GPIO
- Measuring Power and Going to Sleep
- ADC with Delay, Visualization
- SAM L21 Low Power Examples and Training Material
- Configuring the SPI for the EDBG DGI
- Implementing the Data Streamer Protocol
The following series of videos shows you how to use Atmel START, the Advanced Software Framework 4 (ASF4), and the Atmel Studio IDE to develop and debug a project for the SAM L21 microcontroller.
Glen also demonstrates many valuable tips and tricks for the Atmel Studio IDE. For example: Do you know what "F1 datasheet help" is? Watch video eight to see it in action.
Training Videos
Introduction to the video series
Hello World!
- Create a project from scratch using the Atmel START graphical project configurator.
- Add a Universal Synchronous Asynchronous Receiver Transmitter (USART) driver to the project.
- Use ASF4 example code to send a message to a serial terminal over the USART.
Best Practice Code Cleanup
- Move USART ASF4 example code into main.c.
Configuring and Reading the ADC
- Add and configure an Analog-to-Digital Converter (ADC) driver to the project.
- Add ADC example code.
- Measure the analog output from the light sensor on the I/O1 Xplained Pro board.
- Use an I/O view window to display the ADC Result register.
ADC with Delay, Visualization
- Add and configure a Delay driver to start an ADC conversion.
- Add code to the ADC callback function for the Interrupt Service Routine (ISR).
- Display ADC result values on a serial terminal and graph with the Data Visualizer.
ADC with Timer Callback, Visualization
- Add and configure a Timer driver to start an ADC conversion.
- Add Timer example code.
ADC Timer GPIO
- Use a SAM L21 General Purpose Input/Output (GPIO) pin to measure the ADC conversion time.
- Plot the conversion time in the Data Visualizer.
- Embedded Debugger (EDBG) GPIO pins with the Data Gateway Interface (DGI).
Measuring Power and Going to Sleep
- Put SAM L21 into Sleep mode.
- Configure Timer and ADC to run in Sleep.
- Use the Data Visualizer to measure power consumption.
ADC with Delay, Visualization
- Download the Low power example project from Atmel START and import it into Atmel Studio.
- The Data Visualizer is used to display the power consumption.
- The USART is used to temporarily wake the SAML21 from sleep.
- A low power SleepWalking project is also demonstrated.
SAM L21 Low Power Examples and Training Material
- Add temperature sensor middleware.
- Add temperature sensor code.
- Use a watch window to view temperature sensor data.
Configuring the SPI for the EDBG DGI
- Add and configure an Serial Peripheral Interface (SPI) driver for the data stream module in the Data Visualizer.
- Embedded Debugger (EDBG) SPI pins with the Data Gateway Interface (DGI).
- Add SPI initialization example code.
Implementing the Data Streamer Protocol
- Add example code to implement the data streamer protocol.
- Use the data stream module to send temperature and light sensor measurements to the Data Visualizer.