3rd Party Utilities to use with Microchip Software

Last modified by Microchip on 2026/01/09 08:13

Other Software You May Find Useful

This is a collection of third-party utilities that we have found to be useful.  These are not Microchip products and we cannot endorse or support them.  These links are provided for your convenience only.


Terminal Emulators

A "terminal emulator" is a software application that emulates a text terminal or system console. Think of the old CRT displays used to interface with a mainframe in the 1980s.

Today, embedded developers can use a terminal emulator to send and receive ASCII characters or data via a serial port (UART) on the development board.

There are many different terminal emulation programs to choose from. The following are a couple of examples that have worked well for us.

generic image of old computer

Back to Top


CoolTerm

Runs on:

  Windows®
  Mac®
  Linux®

Download CoolTerm.

 

screen shot of the coolterm emulator

Back to Top


Tera Term

Runs on:

  Windows

Download Tera Term.

generic screen shot of teraterm

Back to Top


Static Analyzers

Fun With Static Analyzers!

Anyone who writes code, either professionally or as a hobby, has encountered the pain of debugging an issue that later proves to be caused by a well-known, common programming mistake. Some of us thrive on the thrill of hunting down and squashing these bugs but most of us would prefer to prevent these problems from occurring in the first place.

What if there were tools that could help us identify and fix these common bugs before they became a thorn in our side? What if there were tools to make the code more readable for other humans out there? Static-analysis tools are here to the rescue and one of them has caught our attention lately. Clang-tidy is part of the clang-based static-analysis tool suite, along with the more powerful Clang Static Analyzer and Clang Format tools. Although clang-tidy is presented as a C++ linter tool, it is definitely more than that, providing a framework for running robust analysis on C or C++ code. The errors reported by the tool can help you solve various bugs or fix coding-style issues.

“How can I use the clang-tidy on my code?” “Where can I get the tool?” “Where can I go to get more information?” Keep reading and your questions will be answered.

Back to Top

Using clang-tidy

Clang-tidy is currently available as a command-line tool. To run basic checks on source code files, you can:

  • Instruct clang-tidy what file to analyze.
  • Select which checks to run with the –checks option.
  • Specify, at the end of the command line, the compilation options that are used to build the code (for example, include directories or reprocessor macro definitions).

A simple example of running checks in the clang-analyzer category:
To list all available checks, use the –list-checks option.

When running checks, clang-tidy generates warnings for your code. These warnings identify the places in your code where the check rule matched.

An output example reporting a place where the C++ auto specifier should be used:

As we mentioned earlier, you have the option to automate the process of fixing the potential problems that are detected by adding the –fix option to the command line.

The power of clang-tidy stands in its ability to be easily extended and adapted to detect new issues that may interest you. For that, custom checks can be added to clang-tidy by following their tutorial. The framework facilitates adding new checks through helper Python scripts that create the skeleton source files with classes where the checks will be implemented. The interface that Clang presents in these extension modules gives you access to the Abstract Syntax Tree (AST) level and thus offers the opportunity to implement powerful checks on your code.

Back to Top

Where to Get and Build It

Clang-tidy is part of the clang release and pre-built binaries are available.
Source code can be found in the extra Clang tools (clang-tools-extra) LLVM repository, git mirror. After cloning the tree, the tool can be built as a standalone target following their instructions.

Back to Top

Give it a Try

To conclude, clang-tidy brings a series of benefits to the development process such as: identifying and fixing suspicious coding constructs or even bugs, improving quality through code style checks, and the opportunity to expand the checking features to custom requirements. Give it a try on your MPLAB® XC application code and tell us what you think in the Microchip forums! Also, which other static analyzers have you tried?

Back to Top


Anaconda® Python Distribution

Anaconda® is a free and open-source distribution of Python. It also includes a package manager and Jupyter Notebook. Jupyter Notebook is an application that enables you to interact with a running Python program (provide input and observe output).

All Microchip Secure Products Group products are interfaced through the CryptoAuthLib (CAL) library. Python CrytoAuthLib (pyCAL) is the same library wrapped up for Python. As a result, all current and future Microchip Secure Products Group products are supported through either embedded C code (CAL) or high-level Python code (pyCAL). All interactive tools are built on top of pyCAL.

 

Anaconda logo

Back to Top

Installing Anaconda


On the Anaconda download page, click on your operating system's icon. All the steps followed here are for Windows but should be similar for other operating systems.

image show the 3 major operating system logo windows, Linux, and macOS


Anaconda has both 32-bit and 64-bit installers for different platforms. Download the latest Python 3.x version for your platform.

images shows selecting Python version 3.7


Once the installer is downloaded, double-click it to start the setup window as shown in the accompanying figure and click Next.

the Anaconda installer


It will take you to the user agreement page, click I Agree to proceed.

Anaconda user agreement


Select the Installation type and then click Next.

select the just me install type


Click the Next button for the default installation directory, otherwise choose the installation directory by clicking the Browse button and then click Next.

shows the default directory location


Make sure to have the check box for the Register Anaconda as my default Python 3.x selected and click Install.

select to Register Anaconda as my default Python 3.x


The windows in the following images show the status of the installation. Click Next once the installation is complete.

wait for the bar to show the install is complete
when done next next


Uncheck both checkboxes and click Finish to complete the installation.

the finish screen, hit finish to complete

Back to Top


Installing the AWS Command Line Interface (CLI) from Anaconda

The Amazon Web Services (AWS) CLI is a unified tool to manage your AWS services. You can control multiple AWS services from the command line and automate them through scripts. Refer to the "Install or update the latest version of the AWS CLI" page for more details.

The AWS CLI is installed using pip in the Anaconda environment.

Open Anaconda Command Prompt.

open an Anaconda command prompt


Run pip3 install awscli.

run pip3 install awscli

Back to Top