Enter a brief description of your changes
(Required)
Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
MPLAB® X IDE Debug Toolbar
Last modified by Microchip on 2024/06/24 06:30
The debug toolbar will not be visible when you first launch MPLAB® X IDE. It will appear automatically when you start a debug session.
Information
Keyboard shortcuts may be added or modified.
Finish Debugger Session
Menu: Debug > Finish Debugger Session
Keyboard: Shift+F5
Ends the current debug session and closes the connection to the debug tool.
If you are running multiple debug sessions simultaneously, to end a specific session:
Open the Sessions window by choosing Window > Debugging > Sessions Alt+Shift+6
Right-click the debugging session you want to stop and choose Finish from the pop-up menu.
Pause
Menu: Debug > Pause
Keyboard: Ctrl+Alt+8
Pauses the debugging operation without finishing the session. Debug windows such as memory views and watches will be updated to reflect the current state of the device.
Reset
Menu: Debug > Reset
Keyboard: None
Performs processor reset. Additional resets, such as POR/BOR, MCLR, and System, may be available, depending on the device.
Continue
Menu: Debug > Continue
Keyboard: F5
Resumes debugging until the next breakpoint or the end of the program is reached.
Step Over
Menu: Debug > Step Over
Keyboard: F8
Executes one source line of the program. If the line is a function call, executes the entire function then stops.
Step Into
Menu: Debug > Step Into
Keyboard: F7
Executes one source line of the program. If the line is a function call, executes the program up to the function's first statement and stops.
Step Out
Menu: Debug > Step Out
Keyboard: Ctrl+F7
Executes one source line of a program. If the line is a function call, it executes the functions and returns control to the caller.
Run to Cursor
Menu: Debug > Run to Cursor
Keyboard: F4
Runs the current project to the cursor's location in the file and stops program execution.
Set PC at Cursor
Menu: Debug > Set PC at Cursor
Keyboard: None
Sets the program counter (PC) value to the line address of the cursor.
Focus Cursor at PC
Menu: Debug > Focus Cursor at PC
Keyboard: None
Moves the cursor to the current PC address and centers this address in the window.
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.