Introduction to Device Family Packs (DFPs) in MPLAB® X IDE

Last modified by Microchip on 2025/11/03 09:58

Introduction to Device Family Packs

Watch this video for a comprehensive tutorial on Device Family Packs (DFPs) or continue reading all about DFPs.

A Little DFP History

In the past, Microchip’s MPLAB® X Integrated Development Environment (IDE) and MPLAB XC Compilers came only with built-in support for Microchip devices that were available at the time of their release. This meant that these tools consisted of a single convenient package to download and install, but it also meant that when you wanted to commence projects targeting newly released devices, you had to wait for a new MPLAB X IDE and a new version or part-support update of your compiler before you could proceed.

Now device support is no longer built into MPLAB X IDE or MPLAB XC Compilers, but is installed into these tools in the form of DFPs. These DFPs provide information to tools about the devices used in your projects. This page discusses the advantages that these packs offer.

To see the version when specific tools began supporting DFPs, consult the Minimum Tool Versions Using Packs table below.

Minimum Tool Versions Using Packs

ToolVersion
MPLAB X IDE5.40
MPLAB XC82.20
MPLAB XC161.35
MPLAB XC-DSC3.00
MPLAB XC322.20

Back to Top

The Purpose of DFPs

DFPs are a way of packaging and distributing device support files. They are essentially a structured directory of files that provide information related to each device family. Some of these files are compiler-related device-specific header files, configuration bit data, and libraries; other files relate to device information displayed by MPLAB X IDE and algorithms the IDE uses to program and debug the device. The files are organized in each pack so that the tools know where to find the information they need. A DFP has a version number, just like the compilers and MPLAB X IDE, so that they can be identified.

Before DFPs became available, device information was read from fixed, internal locations in the tool distribution. Now that DFPs are used, MPLAB X IDE and MPLAB XC Compilers have been modified so that they can read the required files on a device-by-device basis and from arbitrary locations that can be selected when building a project. This means that the tools and their support for devices are segregated and each can be updated independently. As new versions of DFPs are made available, they can be used without having to update your current tools.

New releases of DFPs may correct known issues in the resources used by MPLAB X IDE or compilers, however, they will never patch or improve the IDE or compiler applications themselves. This still takes place through the release of new versions of these products.

Back to Top

The Current Usage of DFPs

Although DSPs are still supported in MPLAB X IDE and MPLAB XC Compilers, compilers will no longer be distributed with the DFPs. For details, see the "Using DFPs With a Standalone Compiler" section at the end of this page.

To summarize these updates:

  • DFPs are still used by the compilers.
  • DFPs are no longer shipped with the compilers.
  • If you use MPAB X IDE, there will be no change in your workflow, as the IDE has always managed DFPs for you.
  • If you build on the command line or use build scripts, you will need to manually download and unpack the relevant DFP before you can use the compiler. 

Back to Top

Using DFPs From Within MPLAB X IDE

During the installation of MPLAB X IDE, only those DFPs relating to the device families you require need to be installed. To save disk space and speed up the installation process, you might choose to install no device support at all.

MPLAB X IDE Setup window

When you create a project in MPLAB X IDE, a DFP will be automatically selected if one is available. In the Project Properties dialog, you can see all the available packs and select the one you want to use.

Project Properties dialog

The currently selected pack can be seen on the dashboard.

CRC_test - Dashboard tab

Once you build a project, the pack and version number that was used is displayed in the output view after the build transcript.

CRC_test Output tab

If a pack is not available when you open or create a project, you’ll be prompted to download a relevant pack for the project's device family.

New Project dialog

DFPs that are individually downloaded in this way are stored separately to MPLAB X IDE under .mchp_packs in your user directory, where they can be used by all MPLAB X IDE installations.

The MPLAB X IDE pack manager can be opened from the Tools > Packs menu. From here, you can browse for DFPs by device family. It allows you to see which new and updated DFPs are available, which devices they support, and what changes they implement. Links allow you to install new packs so that they can be used by MPLAB X IDE and compilers.

Tools > Packs menu

Tool packs are also shown by this manager. These contain only firmware and are automatically downloaded by a DFP if they are needed, so you do not usually need to concern yourself with these.

When using MPLAB X IDE, you can create projects for new devices, even if your version of MPLAB X IDE was released before the device became available. To allow this to happen, MPLAB X IDE queries an online index file to fill out the device selection widget in the MPLAB X IDE Project Properties dialog. So, provided your MPLAB X IDE has Internet access, it can find new devices released after your MPLAB X IDE was downloaded and can obtain the latest device support for those devices.

Back to Top

Using DFPs With a Standalone Compiler

The compilers are no longer distributed with the relevant content from the latest DFPs as of MPLAB XC8 v3.10, MPLAB XC-DSC v3.30, and MPLAB XC32 v5.00.

We recommend that you use MPLAB X IDE to install new packs. If required, you can manually download packs from the Microchip Packs Repository page and store them on your host machine in the .mchp_packs directory. They are ZIP files that can be unpacked by most archiver applications, although it is best to unpack and install these using the pack manager in MPLAB X IDE by choosing Install from local source and selecting the .atpack file you have downloaded.

The -mdfp command-line option lets you select an alternate DFP when you build, rather than use the one shipped with the compiler. Specify the path to the compiler directory (either XC8XC16, XC-DSC, or XC32) inside the pack, referenced by version number and device family. Here are some examples of the options for different devices (compiler tools) and host operating systems:

-mdfp=C:/Users/Frank/.mchp_packs/Microchip/PIC24F-MC_DFP/1.2.39/xc16

-mdfp=/Users/john/.mchp_packs/Microchip/PIC16F1xxxx_DFP/1.3.117/xc8

-mdfp=/Users/Jane/.mchp_packs/Microchip/SAMD09_DFP/2.2.110
Information

Note: No xc32 at the end for XC32, xc8 at the end for XC8, and xc16 at the end for XC16 and XC-DSC.

See also Where are Device Family Packs (DFPs) Installed?, "DFPs Components No Longer Bundled With MPLAB XC Compilers".

Back to Top