Project Support Lights in the Project Window of MPLAB® X IDE
Last modified by Microchip on 2024/06/24 06:34
Indicator Lights in the Project Properties and Project Wizard Windows
Tool support for a selected project device is signified by colored circles (lights) in front of the tool name. If you cannot see the colors, hover over a light to pop up text about support.
Table 1: Basic Support Light Definitions
Light | Color | Support |
---|---|---|
![]() | Green | Full (Implemented and fully tested) |
![]() | Yellow | Beta (Implemented but not fully tested) |
![]() | Red | None |
For hardware tools that can be used as either a debugger or a programmer, there are two lights next to the tool name.
Table 2: Two Light Definitions
Light Number | Location | Meaning |
---|---|---|
1 | Left-most light | Debugger Support |
2 | Right of the first light | Programmer Support |