Minor changes are by default collapsed in the page history.
No changes
The page does not exist yet.
Failed to load changes
Version by on
Leave Collaboration
Are you sure you want to leave the realtime collaboration and continue editing alone? The changes you save while editing alone will lead to merge conflicts with the changes auto-saved by the realtime editing session.
Set the Include Directory Path for the MPLAB® XC32 Compiler
Last modified by Microchip on 2023/11/09 09:12
The Include Directory paths are used by the C compiler to find files referenced through #include directives. This is the preferred method of referencing include files that are not at the root of your project directory, as opposed to using relative paths in code: #include "subdirectory/filename.h").
Open the project properties window
Either right-click on the top node of the project in the Project window and select Properties from the pop-up window, or from the File menu, select Project Properties (ProjectName).
If you need to work with Microchip Support staff directly, you can submit a technical support case. Keep in mind that many questions can be answered through our self-help resources, so this may not be your speediest option.