Connecting Atmel-ICE To Data Gateway Interface
Last modified by Microchip on 2023/12/15 20:01
The Atmel-ICE supports a limited Data Gateway Interface (DGI) when debugging and programming are not in use. Functionality, it is identical to the interface found on the Xplained Pro development boards powered by the Embedded Debugger (EDBG) device.
The DGI is an interface for streaming data from the target device to a computer. This is meant as an aid in application debugging as well as for the demonstration of features in the application running on the target device.
DGI consists of multiple channels for data streaming. The Atmel-ICE supports the following modes:
- USART
- SPI
DGI USART Pinout

DGI SPI Pinout