FAQ updates by Components

Last modified by Microchip on 2025/03/10 12:20

AT91Bootstrap


U-Boot


Linux Kernel


Linux Kernel - 3.10


Linux Kernel - 3.18

 
• Using Max Touch
• Crypto hardware acceleration
•  How to use Pulse Width Modulation driver
• How to use the Atmel KMS/DRM LCD driver
• Use of the AT91 ADC driver
• Using ISI (Image Sensor Interface) in Linux4SAM 6.0 and later


Linux Kernel - 4.1

• Using Max Touch
• Crypto Config
• Pwm Faq
• Using Atmel DRMDrive
• Use of the AT91 ADC driver
• Using Ultra Low Power mode 1 (ULP1) on SAMA5D2
• How to use record audio stream with PDMIC
• Using ISI (Image Sensor Interface) in Linux4SAM 6.0 and later


Linux Kernel - 4.4

• Using Max Touch
• Crypto Config
• Pwm Faq
• Using Atmel DRMDrive
• Use of the AT91 ADC driver
• Using Ultra Low Power mode 1 (ULP1) on SAMA5D2
• How to use record audio stream with PDMIC
• Using ISI (Image Sensor Interface) in Linux4SAM 6.0 and later


Linux Kernel - 4.9


Linux Kernel - 4.14

• Using Max Touch
• Crypto hardware acceleration
• USB Gadget Configuration
• How to use Pulse Width Modulation driver
• External Component on External Bus Interface
• How to use the Atmel KMS/DRM LCD driver
• Using the SAMA5D2-compatible Resistive Touchscreen
• Use of the AT91 ADC driver
• Using PTC (Peripheral Touch Controller)
• Using ISC (Image Sensor Controller)
• Use the Wakeup Feature of the Shutdown Controller.
• How to use record audio stream with PDMIC


Linux Kernel - 4.19


Linux Kernel - 5.4


Linux Kernel - 5.10


Linux Kernel - 5.15


Linux Kernel - 6.1


BuildRoot


YoctoProject


OpenWrt


SAM-BA