How to manually select (or enforce) the PDA at boot time
How it works
How to select the PDA at boot time
Starting from Linux4SAM6.0 release, we release a single image named video that includes support for all our PDA screens and HDMI (for SAMA5D4 Xplained only).</br> U-boot has the feature of auto detect at boot time, but this does not work in all possible cases. Some boards may require hardware adjustment for this to work, or, we may want to select hdmi as screen, which is not detectable in U-boot.</br>
Tips: For which screens are supported and how to connect them, check the specific page.
How to manually select the PDA at boot time
If we manually set the _display_ variable in U-boot with the desired PDA/HDMI screen, U-boot will automatically load the correct Device Tree Overlay and the corresponding video mode and will boot the Linux Kernel accordingly.</br> For example, if we want to have U-boot start the kernel with the PDA 5000 enabled, we need to stop the autoboot process, and at the U-boot prompt, issue the command:</br>
</br> We can save this variable in the environment so we do not need to repeat this process on every boot by running the following command:
</br>
Tips: If we have a display that U-boot will autodetect, the display variable will be replaced by the proper one of the detected display.
The table below summarizes the possible values of the _display_ variable:</br>
| value | effect |
| 5000 | Load PDA5000 setup |
| 4300 | Load PDA43XX setup |
| 7000 | Load PDA7000 setup |
| 7000B | Load PDA7000B setup |
| hdmi | Load HDMI setup (only valid for SAMA5D4 Xplained) |
How to manually force U-boot to always load the desired PDA
If we manually alter the U-boot booting command, we can force U-boot to start the kernel with the desired PDA support regardless of the detected PDA.</br> Here is the needed modification:</br>
</br> Will change to:
</br> This will ensure that U-boot will always load pda5 setup regardless of the PDA detected.</br>
The table below summarizes the possible _overlays_ that can be added to the boot command line in U-boot:</br>
| value | effect |
| pda5 | Load PDA5000 setup |
| pda4 | Load PDA43XX setup |
| pda7 | Load PDA7000 setup |
| pda7b | Load PDA7000B setup |
| hdmi | Load HDMI setup (only valid for SAMA5D4 Xplained) |
Practical example with TM4301B screen
The new TM4301B screen is not automatically configured by Linux4SAM 6.0. Its hardware is fully compatible with the previous revision TM4300 or TM4300B screens. So you can follow the above piece of advice to use it by selecting the PDA43XX setup in the table just above which corresponds to "pda4" string:
After having stopped the boot process, you can manually alter the U-boot booting command from the U-Boot prompt. Hereunder are some examples that you can adapt to your boot media and board name.
For the eMMC boot case on SAMA5D2 Xplained board:
saveenv
Or for SD Card boot case on SAMA5D27 SOM1 EK board:
saveenv
Related Topics
Boards
Sam9x60EK
Sama5d27WLSom1EK
Sama5d27Som1EK
Sama5d2PtcEK
Sama5d2Xplained
Sama5d3Xplained
Sama5d4Xplained
Components
Summary
"How to manually select PDA in U-boot