Using systemd

Last modified by Microchip on 2026/01/09 08:12

Introduction

This section provides a guide on configuring and using systemd, the advanced system, and the service manager on the target.

systemd is a robust system and service manager that efficiently manages dependencies between system services by classifying tasks into units and targets. It initiates units and targets automatically during boot or in response to requests from the user or system.

Information

Note: Starting from Linux4SAM 2023.10 release, traditional SysVinit is replaced with systemd as the default.

Features

systemd is almost compatible with most modern features; other notable features include:

  • Reduces boot times through parallel startup procedures
  • Improves dependency management
  • Supports dynamic configuration
  • Provides effective resource management and service monitoring

Prerequisites

 Starting with Linux4SAM 2023.10, we provide and support systemd.
 

Advanced Features

From Linux4SAM 2023.10, Buildroot employs systemd version 252, while the Yocto Project® utilizes systemd version 250 with the additional version label of 250.5+.

Unit Management With systemd

systemd uses a unit as the fundamental object that it controls and operates upon. Though there are many different kinds of units, services are the most prevalent kind (represented by a unit file ending in .service). Various management tasks to control systemd services can be performed using the systemctl command.

Basic Service Management

For instance, to start an egtdemo.service immediately:

systemctl start egtdemo.service

To stop egtdemo.service service: 

systemctl stop egtdemo.service

Similarly, to restart egtdemo.service service: 

systemctl restart egtdemo.service

Enable or Disable Units

Generally, most systemd unit files are not started by default at boot unless it is required, to enable an egtdemo.service to be started automatically on boot: 

systemctl enable egtdemo.service

To disable the started egtdemo.service on boot:

systemctl disable egtdemo.service

To check if a service is enabled or not:

systemctl is-enabled egtdemo.service

To check the status of a specific service, including whether it is running or not: 

systemctl status egtdemo.service

The following is an example of a status log:

 root@sam9x60-curiosity-sd:~# systemctl status egtdemo.service
* egtdemo.service - EGT Application Launcher Service
     Loaded: loaded (8;;file://sam9x60-curiosity-sd/lib/systemd/system/egtdemo.service/lib/systemd/system/egtdemo.service8;;; enabled; vendor preset: enabled)8;;
     Active: active (running) since Fri 2022-04-29 05:41:01 UTC; 57min ago
   Main PID: 205 (egt-launcher)
      Tasks: 2 (limit: 257)
     Memory: 26.6M
     CGroup: /system.slice/egtdemo.service
             `- 205 egt-launcher /opt/applications/resources /usr/share/egt

System State Information

 For example, to obtain every unit file that systemd has listed as active:

systemctl list-units

 To list every unit file that systemd has loaded, though that is listed as not active:

systemctl list-units --all

Back to Top

Log Information

All of the system's journal entries are gathered and managed by the journald systemd component. This is basically a log of information from applications and the kernel.

To see all log entries:

journalctl 

To see journal entries from the current boot, add the -b flag: 

journalctl -b 

To see only kernel messages, such as those that are typically represented by dmesg, you can use the -k flag: 

journalctl -k 

Also, we can limit it to the current boot by appending the -b flag: 

journalctl -k -b 

Back to Top

Managing Network Configurations Using systemd

Default network configuration files are available at /etc/systemd/network (or) /lib/systemd/network directory. 

Information

Note: Files in /etc/systemd/network have a higher priority than those in /lib/systemd/network. 

For Instance, a typical WLAN interface configuration sample is given:

 [Match] 
Name=wlan* 

[Network] 
DHCP=yes 
#Address=192.168.8.2 
#Netmask=255.255.255.0 
#Network=192.168.8.0 
#Gateway=192.168.8.1 

Here, you can see it is configured by default to Dynamic Host Configuration Protocol (DHCP) and dynamically assigns Internet Protocol (IP). 

Wired Network Configuration

To modify DHCP to a static IP configuration for wired interfaces, you can create or edit /etc/systemd/network/10-eth.network file with the following contents:

[Match] 
Name=eth* 

[Network] 
#DHCP=yes 
Address=192.168.7.2 
Netmask=255.255.255.0 
Network=192.168.7.0 
Gateway=192.168.7.1 

Once the configuration is updated for a static IP, reload or restart systemd-networkd using the following command:

systemctl reload systemd-networkd  

or

systemctl restart systemd-networkd

Wireless Network Configuration

To modify DHCP to a static IP configuration for wireless interfaces, you can create or edit /etc/systemd/network/systemd/20-wlan.network file with the following contents:

[Match] 
Name=wlan* 

[Network] 
#DHCP=yes 
Address=192.168.8.2 
Netmask=255.255.255.0 
Network=192.168.8.0 
Gateway=192.168.8.1 

Once the configuration is updated for a static IP, simply reload or restart systemd-networkd using the following command:

systemctl reload systemd-networkd

or

systemctl restart systemd-networkd 

After this, you can observe the static IP assigned to the corresponding interface accordingly as furnished in the following logs:

root@sam9x60-curiosity-sd:~# ifconfig 

eth0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500 
        inet 192.168.7.2  netmask 255.255.255.0  broadcast 192.168.7.255 
        inet6 fe80::691:62ff:fef2:8912  prefixlen 64  scopeid 0x20<link> 
        ether 04:91:62:f2:89:12  txqueuelen 1000  (Ethernet) 

wlan0: flags=4163<UP,BROADCAST,RUNNING,MULTICAST>  mtu 1500 
        inet 192.168.8.2  netmask 255.255.255.0  broadcast 192.168.8.255 
        inet6 fe80::628a:10ff:fed8:9418  prefixlen 64  scopeid 0x20<link> 
        ether 60:8a:10:d8:94:18  txqueuelen 1000  (Ethernet) 

Information

Note: The default static IP configuration given here is just a sample; you can modify it according to your needs.

Back to Top

Related Topics

Boards

Components

Back to Top

Summary

This article provided a comprehensive guide to configuring and using systemd, the advanced system and service manager now set as the default in Linux4SAM releases from 2023.10 onward. systemd’s key features include improved boot times, dynamic configuration, and effective resource management, along with practical instructions for managing services, viewing logs, and configuring network interfaces. The guide also detailed how to enable, disable, and monitor services, as well as how to set up both DHCP and static IP configurations for wired and wireless networks.

Back to Top