Transimpedance (Gm) Amplifier
Last modified by Microchip on 2023/11/09 09:03
The following figure of a circuit shows a transimpedance (Gm) amplifier as formed by an MCP6XXX op amp and R1. It converts the sensor current (ISEN) to a voltage. The capacitor C1 is sometimes needed to stabilize the amplifier when the source has a large capacitance.

Advantages:
- Good impedance buffering of source
- Simplicity
Disadvantages:
- Design may need to be stabilized
Sensor Examples:
- IR smoke detector
- Photodiode
- Photodetector