Pipeline Analog-to-Digital Converter (ADC) Utility Settings

Last modified by Microchip on 2023/11/10 11:07

Device Settings

Analog-to-Digital Converter (ADC)

  • Key ADC setting parameters are found in the first tab.

Pipleline ADC Software ADC setting

I/O

  • Settings that pertain to the device I/O are found in the second tab.

Pipeline ADC software I/O setting

Digital Signal Processing (DSP)

  • Settings that pertain to DSP are found in the third tab. Enabling either the Digital Down Conversion (DDC) or Noise-Shaping Requantizer (NSR) will result in more options being displayed for these functions.

Pipeline ADC software DSP setting

Phase-Locked Loop (PLL)

  • Settings that pertain to the PLL are found in the fourth tab.

Pipeline ADC software PLL setting

Advanced

  • Other settings fall into an advanced category and are found in the fifth tab.

Pipeline ADC software advanced setting

Back to top

Manual Register Manipulation

If custom register manipulation is desired, use the manual register access window to do so. Please note that making changes in this manner is NOT recommended for most users.

Warning

Incorrect changes can result in instability — use caution.

Click on the Register menu and select Manual register access…

Pipeline ADC software menu register access


The RegAccess window will appear.

Pipeline ADC software register number


Select the desired Register Number from the selection box in the upper left area of the window.


Click the Read button in the upper right area of the window to ensure the proper register data is loaded.


Modify the register selected by clicking the checkboxes and/or changing the numeric value of the register.

Information

Any changes will be highlighted in RED.


Write the new value to the device by clicking the Write button in the upper right area of the window.


Back to top

Learn More

Back to top