Step 1: Download and Installation

Last modified by Microchip on 2026/07/28 11:47

Download and Install MPLAB® X IDE

The latest version of MPLAB X IDE is located in the "MPLAB X IDE Downloads, Documentation and Other Resources" section of the "MPLAB X IDE" page. Version 6.30 is currently available; however, version 6.30 or any later release can be used.

MPLAB X IDE Downloads, Documentation and Other Resources section

Once the file is downloaded, open it and proceed with the following installation steps.

In the Setup window, click Next.

Setup window

In the next window, select I accept the agreement and then click Next.

Setup wizard window

Click Next and keep all the other configurations as they are​​​​​​.

Setup wizard MPLAB for VS Code

Setup window Installation Options

Select the applications and Microchip device support as highlighted below, and click Next. 

Setup window Select Application

Information

Note: PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit is a 32-bit MCU, hence, the 32-bit MCUs and MPUs option is selected here. If needed, installation of 8-bit and 16-bit (dsPIC® DSCs) can also be selected.

Now click Next and then the installation will begin.

Setup window Ready to Install

Once the installation is finished, click Finish.

Setup window completing the setup


Install the MPLAB XC32 Compiler

Once the MPLAB X IDE installation process is complete, the setup wizard will automatically navigate to the MPLAB XC32 Compiler installation section. Select Next to proceed.

MPLAB XC Compiler Setup window

Now select I accept the agreement and click Next in the License Agreement section. Also, click Next for the Device Support From Device Family Packs (DFPs), Licensing, Installation Directory, and Compiler Settings sections as shown in the acompanying images. Leave other configurations as is.

License Agreement section

Device Support From Device Family Packs (DFPs) section

Licensing section

Installation Directory section

Compiler Settings section

Now, the MPLAB XC32 Compiler is ready to install. Click Next to install the compiler.

Ready to Install Compiler section

Click Next for the Major Update Warning and Installation Complete - Licensing Information sections.

Major Update Warning section

Installation Complete - Licensing Information section

Information

Note: The Host ID shown in the image was generated automatically by the system. You can continue without altering the generated Host ID.

Click Finish to complete the installation of the MPLAB XC32 Compiler.

Completing the MPLAB XC32 Compiler Setup Wizard

Information

Note: The steps outlined above detail the installation process for the MPLAB XC32 Compiler version 5.00. These steps will also apply to future versions.

 

This is how the MPLAB X IDE looks after installation steps

MPLAB X IDE window

 

Back to Top

Next Page