SAM D21 SysTick Configuration
This section covers basic coding steps required to configure/use the SysTick timer module found in the CPU core of SAM D21 MCUs.

SysTick Operation
The system timer consists of four registers (CTRL, LOAD, VAL, CALIB) which are defined in the CMSIS-Core header file core_cm0plus.h. These registers are located in the SAM D21 System Control Space (SCS) memory region, beginning at address 0xE000E010.
These registers are accessed in C via indirect (pointer) access, using the symbol "SysTick" as a base address pointer to the register set, for example:
SysTick->LOAD = 0x0000FFFF; // Set reload value register
SysTick->VAL = 0; // Reset the counter current value register value
When enabled, the 24-bit timer counter counts down from the value in VAL. When the counter reaches zero, it reloads the value in LOAD on the next clock edge. It then decrements on subsequent clocks. This reloading when the counter reaches zero is called wrapping. When the counter transitions to zero, it sets the COUNTFLAG status bit to '1'. If the TICKINT bit is set, an exception may be generated. Reading the COUNTFLAG status bit clears it to '0'.
Therefore, the SysTick Interrupt Time Period = (LOAD + 1) * CLK Period.
Writing to VAL clears both the register and the COUNTFLAG status bit to zero. This causes the SysTick logic to reload VAL from LOAD on the next timer clock. A write to VAL does not trigger the SysTick exception logic.
Reading VAL returns the value of the counter at the time the register is accessed. Writing a value of zero to LOAD disables the counter on the next wrap. The SysTick counter logic maintains this counter value of zero after the wrap.
The 24-bit counter is clocked by either the CPU clock (AHB clock) or an implementation-defined Reference Clock. The clock source is set by the CLKSOURCE and NOREF flag bits.
SysTick Registers
SysTick_CTRL
SysTick_CTRL is a control and status register that configures the SysTick clock, enables the counter, enables the SysTick interrupt, and indicates the counter status.

bit 16
COUNTFLAG: Indicates whether the counter has counted to 0 since the last read of this register.
1 = timer has counted to 0
0 = timer has not counted to 0
COUNTFLAG is set to '1' by a count transition from 1 to 0.
COUNTFLAG is cleared to '0' by a read of this register, and by any write to the Current Value register.
bit 2
CLKSOURCE: Indicates the SysTick clock source.
1 = SysTick uses the processor clock
0 = SysTick uses the optional external reference clock
If no reference clock is provided, this bit reads as one and ignores writes.
bit 1
TICKINT: Indicates whether counting to 0 causes the status of the SysTick exception to change to pending.
1 = count to 0 changes the SysTick exception status to pending
0 = count to 0 does not affect the SysTick exception status
Changing the value of the counter to '0' by writing zero to the SysTick Current Value register (SysTick_VAL) never changes the status of the SysTick exception.
bit 0
ENABLE: Indicates the enabled status of the SysTick counter.
1 = counter is operating
0 = counter is disabled
SysTick_LOAD
SysTick_LOAD is a counter (re)-load value register. This provides the wrap value for the counter.

SysTick_VAL
SysTick_VAL is the counter current value register.

SysTick_CALIB
SysTick_CALIB is calibration value register. This indicates the preload value required for a 10 ms system clock.

bit 31
NOREF: Indicates whether an IMPLEMENTATION DEFINED reference clock is provided.
1 = the reference clock is not implemented
0 = the reference clock is implemented
When this bit is '1', the CLKSOURCE bit of the SysTick_CTRL register is forced to 1 and cannot be cleared to 0.
bit 30
SKEW: Indicates whether the 10 ms calibration value is exact.
1 = 10 ms calibration value is inexact, because of the clock frequency
0 = 10 ms calibration value is exact
bit 23:0
TENMS: Optionally, holds a reload value to be used for 10 ms (100 Hz) timing, subject to system clock skew errors. If this field is zero, the calibration value is not known.
SysTick Initialization
As the Reload and Current Value registers are undefined at reset, the SysTick setup code needs to be written in a certain sequence:
- Disable the SysTick module
- Program the Reload Register
- Clear the Current Value Register
- Enable the SysTick Module
The following example initializes the SysTick Module to generate interrupt requests every millisecond, given a CPU Clock of 1 MHz:
SysTick->CTRL = 0; // Disable the SysTick Module
SysTick->LOAD = 999UL; // Set the Reload Register for 1mS interrupts
NVIC_SetPriority(SysTick_IRQn, 3); // Set the interrupt priority to least urgency
SysTick->VAL = 0; // Clear the Current Value register
SysTick->CTRL = 0x00000007; // Enable SysTick, Enable SysTick Exceptions, Use CPU Clock
NVIC_EnableIRQ(SysTick_IRQn); // Enable the SysTick Interrupt (Global)
CMSIS SysTick Functions
SysTick configuration is also supported via available CMSIS functions in the core_cm0plus.h file. The following code example uses the SysTick_Config() function, which initializes SysTick and its interrupt (priority level = 3), and starts the timer. The counter is in free running mode to generate periodic interrupts.
SysTick_Config(1000UL);
NVIC_EnableIRQ(SysTick_IRQn);
SysTick Debugging
The SysTick registers may be viewed in the Atmel Studio 7 I/O Debug window as shown. Note that the Arm®-defined SysTick register names are shown:
- SysTick_CTRL = CSR (Control & Status Register)
- SysTick_LOAD = RVR (Reload Value Register)
- SysTick_VAL = CVR (Current Value Register)
- SysTick_CALIB = CALIB (Calibration Register)