SAMA5D2 Series Boot Process
Introduction
This training explains the boot process of the Microchip Technology SAMA5D2 series microprocessor units (MPU), which are Arm® Cortex®-A5-based, from reset to running an operating system (embedded Linux® or RTOS) or application. The boot process begins with the MPU’s power-on reset and progresses in stages reading binary files from external Non-Volatile Memory (NVM) and loading them into volatile memory (internal Static RAM (SRAM) and external Dynamic RAM (DRAM)).

The first-stage bootloader, located in the MPU’s internal ROM (also known as Boot ROM), performs basic initialization and configuration of the device. Its main purpose is to locate a valid second-stage bootloader and read it from external NVM and store it in the MPU’s internal SRAM.
The second-stage bootloader continues the initialization and configuration of the MPU. Its main purpose is to read the third stage binary (bootloader, operating system or application), located in external NVM, and store it in external DRAM. The third stage can be one of the following:
- Third-stage bootloader (for example, Das U-Boot)
- Linux operating system directly (does not require a third-stage bootloader)
- MPLAB® Harmony v3 Software Framework application
- Real Time Operating System (RTOS)
- Turn over control to a debugger (JTAG) (no application is loaded)
Each stage is customizable. The second and follow-on stages are external programs (available as source code) that are configured and compiled by the developer. During development and debugging, the resulting binary files can be stored in an external NVM using a debug probe and the SAM-BA® In-System Programmer utility program or copied to a detachable storage device, such as an SD memory card.
The developer must be knowledgeable of the MPU’s boot process so that each stage is configured and compiled as required by the operating system or application.
References
- SAMA5D2 series Data Sheet – Section 17. Standard Boot Strategies
Processor Reset
The MPU begins the boot process upon reset. The Reset Controller (RSTC) handles all reset events of the device.

Reset Controller Block Diagram
The RSTC responds to the sources listed in the SAMA5D2 Series Processor Reset table (below) and asserts internal signals:
- Processor Reset – resets the processor and embedded peripherals
- Backup Reset – resets all peripherals powered by VDDBU

SAMA5D2 Series Processor Reset
The RSTC reports which reset occurred last in the RSTC Status Register.
The MPU’s Program Counter (PC) is reset to 0x0000 0000 and will begin executing the first-stage bootloader located in internal Read-Only Memory (ROM).

MPU program counter resets and begins execution
First-Stage Bootloader
MPUs contain an internal ROM (also known as Boot ROM) that contains the first-stage bootloader. It is the program that begins executing when the MPU is reset.
The purpose of the first-stage bootloader is to:
Initialize processor and master clocks
Read the Boot Configuration Word
If (valid code found) in external NVM, then:
- Load the second-stage bootloader at91bootstrap into internal SRAM
- Remap internal SRAM to address 0x0
- Reset the PC to 0x0 and jump
Else if (no valid code found) start the SAM-BA monitor
Let’s look at each of these steps in more detail.
Initialize Processor and Master Clocks
Upon reset, the 12 MHz RC oscillator (Clock Generator module embedded in the Power Management Controller (PMC)) performs a fast start-up to start the system. Next, the first-stage bootloader initializes the PLLA phased-locked loop. When it is stabilized, the PLLA is the source for the Master Clock (MCK) and Processor Clock (PCK).
Read the Boot Configuration Word

First-stage bootloader reads the boot configuration word
The first-stage bootloader initially reads the Boot Configuration Word located in the Secure Fuse Controller (SFC).
The Disable Read of the Boot Sequence Controller Configuration Register (DISABLE_BSCR) bit is tested.
- If DISABLE_BSCR = 1: the Boot Configuration Word read from the SFC will be used.
- If DISABLE_BSCR = 0 (default): read the Boot Sequence Controller Configuration Register (BSC_CR)
- If BUREG_VALID = 0: the Boot Configuration Word read from SFC will be used.
- If BUREG_VALID = 1: Read the Backup Register Index (BUREG_INDEX) value and read the Boot Configuration Word from BUREG_n.
The BUREG is located in SRAM in the Security Module (SECUMOD). The registers will retain their value if VDDBU is powered.
The Boot Configuration Word customizes the first-stage bootloader. The following items can be configured:
- Configure the I/O Set where the external memories are connected
- Enable/disable boot on selected memories
- Configure the UART port for console serial communications
- Configure the JTAG port for debugging

Details of boot configuration word
Details of the Boot Configuration Word are shown in the figure above and a short description, with default bit settings, is shown below:
- SECURE_MODE: Enable Secure Boot mode (default: disabled – standard boot sequence)
- DISABLE_MONITOR: Disable SAM-BA Monitor (default: disabled – if no boot file found, launch SAM-BA Monitor)
- DISABLE_BSCR: Disable read of Boot Sequence Controller Configuration Register (BSC_CR) (default: disabled – Read the BSC_CR to determine if Backup Register Valid (BUREG_VALID))
- QSPI_XIP_MODE: Enable XIP mode on QSPI Flash (default: disabled – Access in QSPI mode)
- EXT_MEM_BOOT_ENABLE: Enable Boot on external memories (default: disabled – external memory boot disabled)
- JTAG_IO_SET: Select pins used for JTAG access (default: use JTAG I/O Set 1)
- UART_CONSOLE: Select/disable UART I/O Set for console terminal (default: use UART1 I/O Set 1)
- SDMMC_1: Disable SDCard/e.MMC boot on SDMMC_1 (default: boots on SDMMC_1 using SDMMC_1 PIO Set 1)
- SDMMC_0: Disable SDCard/e.MMC boot on SDMMC_0 ((default: boots on SDMMC_0 using SDMMC_0 PIO Set 1)
- NFC: Select/disable Parallel Input/Output Controller (PIO) Set used for NFC Boot (default: use NFC PIO Set 1)
- SPI_1: Select/disable Parallel Input/Output Controller (PIO) Set used for SPI_1 Boot (default: use SPI_1 PIO Set 1)
- SPI_0: Select/disable Parallel Input/Output Controller (PIO) Set used for SPI_0 Boot (default: use SPI_0 PIO Set 1)
- QSPI_1: Select/disable Parallel Input/Output Controller (PIO) Set used for QSPI_1 Boot (default: use QSPI_1 PIO Set 1)
- QSPI_0: Select/disable Parallel Input/Output Controller (PIO) Set used for QSPI_0 Boot (default: use QSPI_0 PIO Set 1)
If (valid code found) in external NVM, then:
If valid code is found, the second-stage bootloader, at91bootstrap, is read from the external NVM and stored in internal SRAM.
There are two types of valid code detection:
- Arm Exception Vectors check
- boot.bin File check
The type of detection that will be used is determined by the external NVM media type.
Load second-stage bootloader at91bootstrap into internal SRAM
If at91bootstrap, is found in external storage such as NAND Flash, QSPI Flash, etc., it must follow the first method of valid code detection: Arm exception vectors check.
If at91bootstrap, is found in SD memory card or e.MMC memory, it must follow the second method of valid code detection: boot.bin file check. It must be stored in the root directory of a FAT formatted file system.

Card-detect pin must be active for only memory devices
Remap internal SRAM to address 0x0
Once the valid code is loaded into internal SRAM, the first-stage bootloader remaps internal SRAM to address 0x0.

First-stage bootloader remaps internal SRAM to address 0x0
Reset the PC to 0x0 and jump
The MPU begins the execution of the valid code.
Else if (no valid code found), start the SAM-BA Monitor program
If the first-stage bootloader does not find valid code in any external NVM, it begins the execution of the SAM-BA monitor.
In accordance with the Boot Configuration Word, the SAM-BA monitor can be enabled or disabled. If there is no Boot Configuration Word stored in SFC, the SAM-BA monitor is enabled by default.

Recommended that SAM-BA monitor is disabled in production code to enhance security
Second-Stage Bootloader
The second-stage bootloader, at91bootstrap, is an external program, available in source code format. It is written and maintained by Microchip Technology and hosted on GitHub. The developer downloads, configures, and builds it according to the project’s hardware and software requirements.
at91bootstrap is stored in external NVM memory. The first-stage bootloader initializes external NVM and stores at91bootstrap into internal SRAM. Once it is loaded, the first-stage bootloader remaps internal SRAM to address 0x0, resets the PC to 0x0, and jumps.
The purpose of the second-stage bootloader, at91bootstrap, is to:
- Initialize the Main Oscillator
- Initialize external volatile and NVM interfaces, controllers, and memory
- Configure peripherals
- Load one of the following from external NVM into external volatile memory (DRAM) (main memory) and jump to:
- Third-stage bootloader (for example, Das U-Boot)
- Linux operating system directly (does not require a third-stage bootloader)
- MPLAB® Harmony v3 Software Framework application
- Real-Time Operating System (RTOS)
- Turn over control to a Debugger (JTAG) (no application is loaded)

SD memory card file system
Third-Stage Bootloader
A third-stage bootloader continues initializing peripherals on the MPU and facilitates the loading of the Embedded Linux operating system. The use of a third-stage bootloader is optional.
Das U-Boot
Das U-Boot (often abbreviated U-Boot) is an open-source bootloader used to configure and initialize peripherals and load and run the Linux operating system. It is written and maintained by a large open-source community and hosted on GitHub. The developer downloads, configures, and builds it according to the project’s hardware and software requirements.
U-Boot is especially helpful during development. During board bring-up, U-Boot can be a simpler software to configure compared to Linux. Also, it allows you to run scripts providing a more flexible tool for experimentation during development. It allows multiple options to load the kernel or root file system. You can interrupt the boot process and enter commands via a Command-Line Interface (CLI). Visit the U-Boot "Command-line Parsing" page.
However, U-Boot does add time to the boot process. To speed up the boot process, or if the application is limited on memory or minimal boot time is important, the developer may elect to boot the Linux kernel directly using at91bootstrap.
If an application is to be loaded, such as from the MPLAB® Harmony v3 Software Framework, it can be booted directly by the second-stage bootloader, at91bootstrap.

Application loaded and booted directly by the second-stage bootloader
Embedded Linux
Embedded Linux is a popular choice for MPU development. It is much more than just an operating system. It is a large collection of software libraries, device drivers, networking stacks, software applications, and tools to choose from. There are thousands of developers contributing to its open-source model. There is a large online community providing tutorials and answering questions in forums to aid the developer.

Embedded Linux is a popular choice for MPU development
MPLAB Harmony v3 Software Framework
MPLAB Harmony v3 Software Framework is a comprehensive collection of software libraries and tools for the software developer to manage, configure and generate source code for Microchip Technology branded MPUs. The developer can choose the level of development that best suits their application. The framework includes many example applications to enable the developer to get started quickly.
Real-Time Operating System (RTOS)
RTOS provides multitasking, real-time scheduling, multi-thread capabilities, inter-task communications, and many more features. They also greatly simplify the development of complex applications. RTOSs offers much more than just an operating system; they also include software libraries, device drivers, networking stacks and a large selection of software applications.
Turn Over Control to a Debugger
This option is used for development. Before control can be turned over to a debugger, the MPU requires initialization and configuration of memories from the first- and second-stage (at91bootstrap) bootloaders. Once the MPU is initialized and internal and external memories are configured, the boot process ends. At this point, the debugger can load binary files and run them.
Summary
This training explained the boot process of a Microchip Technology SAMA5D2 series Arm Cortex-A5 processor-based MPU from reset to running an operating system (embedded Linux or RTOS) or application.