SAMA5D29-Curiosity – Configure and Build at91bootstrap for a MPLAB® Harmony v3 Project with MPLAB® X IDE
Contents
Introduction
This training topic describes how to configure and build at91bootstrap for loading and debugging an MPLAB® Harmony v3 project on the SAMA5D29-Curiosity Development Board (P/N: EV07R15A) using the MPLAB X Integrated Development Environment (IDE).
Background
The at91bootstrap is used by MPLAB X IDE to initialize Dynamic RAM (DRAM) so that it can continue loading the MPLAB Harmony v3 Software Framework project binary (harmony.bin). Once the project has been loaded onto the SAMA5D29-Curiosity, MPLAB X IDE can be used to develop and debug the application.
Prerequisites
- MPLAB X IDE Installed
- XC32 installed
Download at91bootstrap
Create a Project Directory.
For this training topic, we will name our project directory “at91bootstrap”.
Download or clone at91bootstrap version 4.
Download or clone from the Linux4sam GitHub repository.
Open Project at91bootstrap
From MPLAB X IDE, select File > Open Project…
An Open Project dialog is displayed.
Find and select the at91bootstrap project directory.
Click on the Open Project button.
The at91bootstrap project will be displayed in the Projects pane (upper left) and the at91bootstrap – Dashboard pane (bottom left).
Configure at91bootstrap Project Properties
Open at91bootstrap Project Properties
Open the at91bootstrap Project Properties using one of the following methods:
- In the Projects pane, highlight at91bootstrap and click on the wrench icon in the at91bootstrap - Dashboard.
- In the Projects pane, right-click on at91bootstrap and select Properties from the menu.
The Projects Properties – at91bootstrap dialog box opens.
In the Device dropdown box, select ATSAMA5D29

Highlight the latest DFP and click on the Apply button.
This will update the configuration to the latest DFP.
Configure the XC32 Compiler
In the Categories pane, select Makefile.
Enter the following text in the Build command and Debug build command boxes:
make CROSS_COMPILE="C:/Program Files/Microchip/xc32/v4.35/bin/bin/pic32c-"
Enter the following text in the Clean command box:
make mplabclean CROSS_COMPILE="C:/Program Files/Microchip/xc32/v4.35/bin/bin/pic32c-"

Click on the Apply button.
Configure at91bootstrap
In the Categories pane, select Kconfig and click on the Load button.
Find the at91boostrap project directory and select configs directory. Then select sama5d29_curiositysd_uboot_defconfig and click on the Open button.

Observe the following settings:
Expand Primary Operation and then click on the Configure and stop radio button.

Expand DRAM. Next, expand DRAM parts and observe the LPDDR2 AS4C128M32MD2A (SAMA5D29-Curiosity) radio button is selected.

Scroll down and expand Board’s Workaround Options. Expand Workaround for Board Quirks and observe the None Quirks for the board radio button is selected.

Click on the Apply and then the OK button. The Project Properties dialog will close.
Build at91bootstrap
Build at91bootstrap
Build the at91bootstrap project using one of the following methods:
- In the Projects pane, right-click on at91bootstrap and select Build from the menu.
- Click on the Build icon (hammer) in the tool ribbon.
Observe the build is successful.

Note the location of at91bootstrap.elf:
<project_directory>/at91bootstrap/build/binaries/at91bootstrap.elf
Summary
The at91bootstrap has been configured and built to load and debug an MPLAB Harmony v3 Software Framework project using the MPLAB X IDE for the SAMA5D29-Curiosity Development Board.
What’s Next?
Once the at91bootstrap has been configured and built, it can be used with an MPLAB Harmony v3 Software Framework project. When configuring an MPLAB Harmony v3 Software Framework project, at91bootstrap.elf file is configured in the Project Properties as shown in the accompanying example figure.
MPLAB X IDE uses at91bootstrap to initialize DRAM and continue loading the MPLAB Harmony v3 Software Framework project binary (harmony.bin) using a Debug Probe. Once the project has been loaded onto the SAMA5D29-Curiosity, MPLAB X IDE can be used to develop and debug the application.