SAM9X60-EK Evaluation Kit
In this training topic we introduce the SAM9X60-EK Evaluation Kit.
The SAM9X60-EK is designed for evaluating and prototyping with the high-performance, ultra-low power SAM9X60 ARM926EJ-S based microprocessor (MPU) running up to 600 MHz which can be used to develop embedded Linux®, MPLAB Harmony v3 Software Framework, or Real-Time Operating System (RTOS) applications.
For information on Microchip's MPU offerings, visit the microprocessors (MPUs) product page.

What is the SAM9X60-EK?
The SAM9X60-EK Evaluation Kit is a multi-function demonstration and development platform featuring:
- SAM9X60 MPU
- Mass Storage
- Communications
- Debugging
- User Interface
- Expansion
- Power Options
How do I get started?
Start by familiarizing yourself with the SAM9X60-EK Evaluation Kit - Features page and then jump to the SAM9X60-EK Evaluation Kit - Booting Demo Linux Image page.
Where can I get demo images?
Demonstration images for the SAM9X60-EK are available on the Linux4SAM website. Images are available from three build automation systems:
How do I program the SAM9X60-EK?
Demonstration images listed above can be flashed onto an SD memory card (of size 1 GB or higher) using a utility program (such as balenaEtcher) and inserted into the J4 SD memory card slot. This is explained in the SAM9X60-EK Evaluation Kit - Booting from SD Memory Card page.
Where can I get source code?
Source code is available for the SAM9X60-EK at the Linux4SAM GitHub repository.
How do I debug?
There are two methods of debugging the SAM9X60-EK.
- The first method is by JTAG. There are two JTAG interfaces, a 20-pin IDC connecter J23 for the external debugger and an onboard SEGGER J-Link through USB port J22.
- The second method is a Universal Asynchronous Receiver Transmitter (UART) debugger J24.
More information about both methods is available in the "SAM9X60-EK Evaluation Kit - Features" section. Application debugging can also be performed over a TCP/IP connection using the GDB server.
There is also a Serial Debug Port (J24) where you can:
- View the kernel log
- Query processes
- Get information on various internal features of the system
For more information see, SAM9X60-EK - Console Serial Communications.
See the SAM9X60-EK - Booting Demo Linux Image page for more information about the Linux console.
Is there any additional information on the SAM9X60-EK?
Additional information can be found on the SAM9X60-EK product webpage. There you can find:
- User’s Guide
- Design Files
- Manufacturing Files
- Links to component datasheets
Where can I order one?
What is included in the box?
Contents of the box are:
- The SAM9X60-EK baseboard
- USB-A to USB Micro-B cable
- 50-position FFC/FPC cable used for connecting an external display. See SAM9X60-EK - Attaching the TM5000 WVGA Display

What do I need to supply?
For booting demo Linux images, you will need to supply:
- Personal computer (Windows®, macOS®, Linux) running a terminal program
- SD memory card (1 GB or larger)
What's Next?
Learn the features of the SAM9X60-EK on the SAM9X60-EK Evaluation Kit - Features page.