SAMA5D29-Curiosity – Booting Demo Linux® Image
Introduction
This training topic lists step-by-step instructions for booting a demonstration Linux® image written to a micro-SD memory card on the SAMA5D29-Curiosity Development Board.
There are several pre-compiled demonstration Linux images available from the Linux4sam website.
What you will need:
- SAMA5D29-Curiosity Development Board (P/N: EV07R15A)
- Personal computer (Windows®, macOS®, Linux) running a terminal emulation program
- USB-to-Serial 3.3 or 5.0 VDC TTL Level adapter with a 6-pin single-in-line 0.1” pitch connector
- To power the SAMA5D29-Curiosity you will either:
- Connect a USB Type-C cable to USB-A port (J1) (included)
- Connect an external 5 VDC power supply to DC Jack (J2)
- Micro-SD memory card (1 GB or larger)
Prerequisites
- Familiarity with the features of the SAMA5D29-Curiosity Development Board.
- Knowledgeable of the SAMA5D2 Series Boot Process.
Hardware
For this training topic, you will use the SAMA5D29-Curiosity Development Board (P/N: EV07R15A) .
SAMA5D29-Curiosity Demonstration Board
Setup the SAMA5D29-Curiosity as listed below:
Jumpers
- Set the jumpers to their default positions as shown in the “Jumper Summary” section in the “SAMA5D29-Curiosity – Features” page.
- OPEN Jumper J10 to disable Serial Quad I/O (SQI) Flash Boot
Power
- Apply power to the development board by connecting either :
- USB Type-C connector to USB-A port (J1), or
- Applying 5.0 VDC to DC Jack (J2).
Download a Demonstration Image
The latest demonstration images for the SAMA5D29-Curiosity are available on the Linux4sam website. There you will find three sets of images created from the following build systems:

You will find headless and graphics versions. The headless versions only require serial communications between a host computer running a terminal emulation program and the target console. The graphics version works with displays such as the High-performance WVGA Display Module with maXTouch® (Part Number: AC320005-5) and High-Performance WQVGA Display Module with maXTouch (Part Number: AC320005-4).
For this training, we will use the Buildroot headless version. Download the image and follow the steps below.
Load image onto SD Memory Card
To boot Linux from a micro-SD memory card, perform the following steps.
You will write the image to the micro-SD memory card using the balenaEtcher utility program. balenaEtcher is a cross-platform utility program used for writing image files onto storage media.
Select Image
Locate the directory where the image has been stored. There is no need to un-compress the image file. The balenaEtcher utility program can handle compressed image files.

Select Target
Select the micro-SD memory card.

Flash!
Finally, write the image to the micro-SD memory card. This will take some time, be patient.

Insert the micro SD Memory Card
Insert the micro-SD memory card into the slot (J6) located on the bottom side of the development board.
Terminal Emulation Program
Download, install, and configure a Terminal Emulation program onto your host computer. There are several choices for terminal programs for Windows, macOS, and Linux.
Jumpers
Ensure that the Serial Quad I/O (SQI) Flash Boot jumper (J10) is OPEN.
Connect to UART Debug Port:
Connect the USB-to-Serial 3.3 or 5.0 VDC TTL level adapter to the Serial Debug connector (J28) and the host computer. Take care to align Pin 1 (GND) of the Curiosity board to the adapter Pin 1 (Look for an arrow on the connector and a black wire).
Serial Communication Established
Once you connect the USB-to-Serial adapter to the Host PC, locate the COM Port, open the terminal emulation program, and enter the settings:
- Com Port: as indicated
- Baud: 115200
- Data Bits: 8
- Parity: None
- Stop Bits: 1
Apply Power
Apply power to the development board by either:
- Connect a USB Type-C cable to USB-A port (J1) (included)
- Connect an external 5 VDC power supply to DC Jack (J2)
Boot
Press the START push button (SW3).
Observe the boot log scrolling on the Console. At the end, the command line will prompt the user to log in. Log in as ‘root.’ There is no password required.
Log in for the linux4sam-buildroot-sama5d29_curiosity-headless-2023.10.img:

Observe the RGB LED (D5) flashing blue (heartbeat).
Summary
In this training topic, you booted a demonstration Linux image written to a micro-SD memory card on the SAMA5D29-Curiosity Demonstration Board.