SAMA5D29-Curiosity – Features
Contents
- Introduction
- SAMA5D29 MPU
- Mass Storage
- Communications
- Debugging
- User Interface
- Expansion
- Power Options
- Jumper Summary
- Learn More
Introduction
This topic describes the features of the SAMA5D29-Curiosity Development Board (P/N: EV07R15A) with links to additional information.
Features Summary
The major features of the SAMA5D29-Curiosity are:
- SAMA5D29 MPU
- Mass Storage
- Communications
- Debugging
- User Interface
- Expansion
- Power Options
- Jumper Summary
References

SAMA5D29 MPU
The SAMA5D29 is a high-performance, ultra-low-power Arm® Cortex-A5 CPU embedded microprocessor (MPU) running up to 500 MHz.

Mass Storage
There are three mass storage options available on the development board.

64 Mb Serial Quad I/O (SQI) Flash with EUI-48 and EUI-64 (U9)
U9 is a 64 Mb Serial Quad I/O (SQI) Flash with EUI-48 and EUI-64 memory (Microchip SST26VF064BEUI). It is connected to the Quad SPI Interface 1 (QSPI1) peripheral of the SAMA5D29.
Secure Digital Multimedia Card (SDMMC) (J7)
J7 is a Secure Digital (SD) or MultiMediaCard (MMC) Memory Card slot. It is connected to the Secure Digital MultiMediaCard port 1 (SDMMC1) peripheral of the SAMA5D29.
Micro Secure Digital (J6) (Bottom Side)
J6 is a micro Secure Digital (SD) Memory Card slot mounted on the bottom side of the development board. It is connected to the Secure Digital MultiMediaCard port 0 (SDMMC0) peripheral of the SAMA5D29.
Communications
The SAMA5D29-Curiosity provides wired communications via Ethernet, USB, CAN, and wireless communications from SDMMC slot (J7) and Bluetooth® UART (J8).

Ethernet (J15-J18)
The SAMA5D29-Curiosity contains a 10Base T/100Base-TX Ethernet Reduced Media-Independent Interface (RMII) available on connectors J15, J16, J17, and J18. Microchip provides a wide range of compatible Ethernet daughter boards that can be used for testing and evaluation. See the SAMA5D29-Curiosity User’s Guide for more information.
USB (J1 and J11)
The SAMA5D29-Curiosity features two USB communication ports named USB-A (J1) and USB-B (J11).
The USB-A port (J1) acts only as a USB device interface and is accessed via USB Type-C connector J1.
The USB-B port (J11) acts as a host and is accessed via USB Type-A connector J11.
Controller Area Network (CAN) Flexible Data-Rate (FD)
The SAMA5D29 MPU contains two CAN-FD peripherals. By selecting a CAN-FD compatible mikro Click board™, the CAN-FD interfaces can be evaluated.
MCAN0 signals are routed to the mikroBUS 1 connector (J19) by moving resistors R184 to R181 and R185 to R180. The resistors are located on the bottom side of the development board, below the mikroBUS 1 connector.
MCAN1 signals are routed to the mikroBUS 2 connector (J22) by moving resistors R192 to R189 and R193 to R188. The resistors are located on the bottom side of the development board, below the mikroBUS 2 connector.
Wireless Connectivity
Wireless communications (IEEE 802.11 b/g/n and Bluetooth) can be added to the SAMA5D29-Curiosity by plugging in SD memory card format radio modules such as the ATWILC3000-SD Evaluation Kit (P/N: AC164158) to SD Memory Card slot J7.
Bluetooth modules that support the serial UART interface can connect to the 6-pin header J8.
Debugging
There is one method of debugging the SAMA5D29-Curiosity via JTAG (J27). In addition, a dedicated serial port for debugging and Console Serial Communications (J28).

JTAG (J27)
A JTAG interface to the SAMA5D29-Curiosity is provided by 20-pin connector J27. This facilitates software development and debugging by connecting an external JTAG debugger such as the J-32 Debug Probe or Segger J-Link BASE Debug Probe.
Serial Debug Port (J28)
The Serial Debug Port (J28) is a dedicated TTL-level serial port connection between the SAMA5D29 and J28. A level shifter (U12) allows either 3.3 or 5.0 VDC levels. To interface between J28 and the host computer, you will need a USB-to-Serial (3.3 or 5.0 VDC) TTL level adapter with a 6-pin single-in-line 0.1” pitch connector.
A terminal emulation program running on a host computer provides a user interface to interact with the target console.
User Interface

Red-Green-Blue (RGB) LED (D5)
The SAMA5D29-Curiosity features one RGB LED (D5).
Pushbuttons (SW1-SW3)
The SAMA5D29-Curiosity contains three pushbuttons:
- USER (SW1): User push button is the connector to PIO PA17 and is available for the user’s usage.
- RESET (SW2): Reset push button, when pressed the system resets.
- START (SW3): When pressed it will initiate the PMIC start-up sequence if the buck converters are off. The PMIC will also assert the SAMA5D29 wakeup (WKUP) signal to wake the MPU from a low-power state.
Liquid Crystal Display (LCD) Interface (J23)
The SAMA5D29-Curiosity contains an 18-bit parallel LCD Interface that supports various LCD Displays. The Liquid Crystal Display Controller (LCDC) I/O lines are available on the baseboard 50-pin Flexible Flat Cable (FFC) / Flexible Printed Circuit (FPC) connector J23.
Image Sensor Controller (ISC) Camera Interface (J24) (Not populated)
The SAMA5D29 contains an Image Sensor Controller (ISC) that supports incoming data from a parallel CMOS/CCD sensor. The system supports an active interface and the ITU-R BT 656/1120 422 protocol with an 8-bit or 10-bit data width and raw Bayer format. The ISC I/O lines are available on baseboard 2x15 connector J24 (not populated).
Expansion

mikroBUS™ (J19 and J22)
mikroBUS™ socket is a proprietary communication and plugin standard for small interface boards called Click boards that extends the capabilities of the development board by offering Serial Peripheral Interface (SPI), UART, TWI, and PWM-based sensors and devices. They are made by MikroElektronika, a producer and retailer of hardware and software tools for developing embedded systems.
GPIO/Raspberry Pi Connector(J25)
The SAMA5D29-Curiosity contains a 40-pin GPIO connector (J25) for use. This connector is compatible with the Raspberry Pi expansion header.
Multifunction 20-Pin Connector (J26) (Not populated)
The 20-pin Multifunction connector provides connectivity to alternate functions of certain SAMA5D29 PIOs. One such function is bringing the NAND Flash interface to this connector. Refer to the SAMA5D29-Curiosity User’s Guide for more information.
Tamper (J29) and System Signals (J30) Connectors (Not populated)
The SAMA5D29-Curiosity board provides six tamper pins for static or dynamic intrusion detection on connector J29 (not populated).
Unused I/O signals from the SAMA5D29 are routed to connector J30 (not populated).
| Signal Name | Description |
|---|---|
| JTAGSEL | JTAG boundary scan mode enable |
| RXD | Low-Power Asynchronous Receiver |
| SHDN | Enable/disable external power supply circuit |
| WKUP | Event detection input used to wake up the processor from Shutdown state |
| COMPN | Analog comparator inverting input |
| COMPP | Analog comparator non-inverting input |
Power Options
There are two options to power the SAMA5D29-Curiosity.

USB-A Port (J1)
The USB-A port (J1) is a USB-C connector and can be used as a source of power to the development board. In most cases, this port is limited to 500 mA.
DC Jack (J2)
The SAMA5D29-Curisosity can be powered by an external 5.0 VDC power supply. The connector (J1) is a 2.1 mm coaxial center-positive.
Jumper Summary
The SAMA5D29-Curiosity jumpers are as follows:

Jumper J3 – VDDBU Current Measurement:
- Closed: (default)
- Open: Removing the jumper will remove power to VDDBU and reset the Backup Registers (BUREG) to their initial configuration.
Jumper J10 – Serial Quad I/O (SQI) Flash Boot:
- Closed: enable boot (default)
- Open: disable boot
Jumper J14 – Enable RMII 50 MHz Clock Source:
- Closed: Enables (default)
- Open: Disables
Learn More
- SAMA5D29-Curiosity – Introduction
- SAMA5D29-Curiosity – Console Serial Communications
- SAMA5D29-Curiosity – Booting Demo Linux® Image
- SAMA5D29-Curiosity – Read and Write Boot Configuration Word using SAM-BA ISP
- Developing with Embedded Linux
- Developing Applications with MPLAB Harmony v3 Software Framework for MPUs